Part Number: SN74LVC540A Tool/software: As a representative IC, this is a question about ICs such as the SN74LVC540A that can withstand an input voltage that is higher than the supply power voltage.
I understand that when the supply voltage is 3.3V…
Part Number: SN74LVC540A Other Parts Discussed in Thread: SN74LV540A Hello support member
I downloaded SN74LVC540A.cir from TI homepage. Generated .lib from .cir. I generated .olb from .lib and tried to run circuit simulation.
In the same way, SN74LV540A…
Part Number: SN74LVC540A Hi,
Could you please give me help for IOL and IOH in SN74LVC540A?
1. Datasheet shows IOH and IOL are 24mA at 3.3V of VCC. Would it be total IOH / IOL? or is it mean 1 ch support 24mA?
2. If you have IOL/IOH temperature dependency…
This thread is closed due to inactivity. If you have a question or comment on this topic, please feel free to continue the conversation here -- just don't expect the OP to respond!
Part Number: SN74LV541A Other Parts Discussed in Thread: SN74LV540A , SN74AHC540 , SN74LVC540A Tool/software: Team, customer is looking for p2p compatible(similar output driving strength) with SN74LV541A, but it's an inverting buffer, and there's no upper…
Part Number: SN74LS540 Other Parts Discussed in Thread: CD74AC540 , SN74LVC540A Hi team,
May I know max Io how many currents can be provided? per channel? thanks
Hi Carlos,
Please see attached PCN. It is information only. The datasheet has changed slightly, but the device itself has not changed.
Regards,
Nikki
Texas_Instruments_Datasheet_InformationOnly_20260730000.0.pdf
Hello,
I'm looking for an octal inverting clock buffer. 8 inputs, 8 inverted clock outputs, that can run at up to 20MHz and have a propagation delay of less than 10ns.
I'm thinking the
SN74LVC540A-Q1
will do the job. Are there any better suggestions…
Data /OE Output
0 0 0
0 1 0
1 0 1
1 1 0
This is an AND gate with an inverted input. A single gate can be implemented with the SN74LVC1G97; for many gates, combine inverter and AND devices, e.g., SN74LVC540A and 2× SN74LVC08A.
With an active-high…
Select this link to see answers to common questions, detailed use case implementations, and part recommendations for logic and voltage translation devices. .
Top Logic and Voltage Translation FAQs - All-Time
How does a slow or floating input affect…