Part Number: SN74LXC2T45-Q1 Tool/software: Hi
We are currently using your part TI # SN74LXC2T45QDTTRQ1. We received a part with "1LN" marking and we'd appreciate it if you could confirm whether this marking is correct for this specific part.
This…
Part Number: SN74LXC2T45 Other Parts Discussed in Thread: TXU0202 Tool/software: Hi Team,
Please help to review the design of SPI to RS485 If the schematic has any issues,please tell me.
Part Number: SN74LXC2T45 Tool/software: HI
SN74LXC2T45 Level Shift IC, the datasheet writes Vcco 3V Io Max 24mA. Does it mean that the drive current of A1&A2 can reach Max 24mA or the two together add up to a maximum of 24mA?
Part Number: SN74LXC2T45 Tool/software: We're unable to check the correct part marking for this part number : SN74LXC2T45DCUR .
There's no part marking in TI website and datasheet to check.
Part Number: SN74LXC2T45 We are using SN74LXC2T45.
I use only 1A and 1B
Should I use pull down OR pull up resistor at 2A and 2B. If required, what is the recommended value ?
Part Number: SN74LXC2T45 I am using the SN74LXC2T45QDCURQ1 IC with the following connections:
VCCA connected to +3.3V
VCCB connected to +1.8V
DIR connected to GND (B to A)
Initial testing show correct translation. However, after further testing…
Part Number: SN74LXC2T45 Hi Logic team,
In the datasheet only specifies the input leakage current when Vinput = Vcci. Do you have the test conditions where Vinput is higher than Vcci ?
Rgds, Kelvin
Part Number: SN74LXC2T45-Q1 The datasheet and online look-up tool both show the part marking as 1LL for SN74LXC2T45QDTTRQ1. However, TI sent us parts marked 1LN.
I believe this is the qualification of a new fab location but can you confirm 1LN is a…
Part Number: SN74LXC2T45 Would like your support for component survey below. It is important to Rockwell for component resiliency and risk assessment.
Also please share ROHS3 certificate and Shock & Vibration Document for the same.
Supplier…