Part Number: SRC4382 Hi Team, Need your help on this. Our customer wants some clarification with the way the data and channel status buffer maps of the DIR and DIT were set in Tables 5-8 (Register Pages 1 and 2) of the datasheet. In here bit 0 is defined…
Part Number: SRC4382
Hi Sir
My Application is re-sampling audio input(I2S) from Port A(32kHz~96kHz) to Port B(fixed in 48KHz) .
and set register like below
0x3 <= 8'b00000000
0x4 <= 8'b00000011
0x5 <= 8'b00011000
…
Part Number: SRC4382 Hello
In order to keep the integrity of the digital inputs, could you please forward the signals coming from the DIR inputs and Port A I2S directly to Port B without passing through the ASRC.
Example: Input DIR SP/DIF 48kHZ,Out PORTB…
Part Number: SRC4382 In order to keep the integrity of the digital inputs, could you please forward the signals coming from the DIR inputs and Port A I2S directly to Port B without passing through the ASRC.How to configure the software?
Part Number: SRC4382 We are seeing similar issues to the thread below, where the I2C bus locks up. Replacing the SRC4382 resolves the problem. The issue may be batch related as we have used this part in the existing design for quite a few years now and…
Hi Shu-Cheng,
Do you have any follow-up questions about using the SRC4382 for this use case? As Steve mentioned in the earlier note, the second block diagram is very much possible to be configured using the SRC device but the input/output sampling rate…
Part Number: SRC4382 On the AES output pin 34, the carrier is slipping and at the same time the down-stream result is low level audible noise, much like pink noise bursts.
This occurs with or without an AES input to the SRC4382.
The master clocking…
Part Number: SRC4382 Hi,
I have the EVM for the SRC4382 but I don't have the CD with the drivers and software (It was here in the university, and someone have lost it). I have tried to stablish the comunication with the AIC3254 CS software (I saw somewhere…
Part Number: SRC4382 Hello.
I have a simple question, I hope.
In the SRC4382, how is the output sample rate from the sample-rate-converter determined?
On p.33 of the datasheet, this signal is shown as INT_SYNC, but it is not mentioned elsewhere how this…