Part Number: TAS2110 Hi,
Based on below table (VBAT) limiter minimum threshold, the lowest Vbat is 2.5V but base on the recommended operating condition, the VBAT min is 2.7V. which one should I refer to??
Part Number: TAS2110
Hi, Team
output is 3W/4ohm, 10uH+0.68uF, When boost enable, the test result is below
When boost disable
How to solve this problem?Thanks
Part Number: TAS2110 Other Parts Discussed in Thread: TAS2563 , TAS2505 , TAS2562 , TAS2557 , TAS2558 Hello, I have custom carrier board for Jetson Nano (kernel 4.9.253) with TAS2110 audio amplifier. Firstly I made test manually - play I2S sound and configure…
Part Number: TAS2110 Hi Team,
The current battery voltage is around 3.3V, OCP will active, I Hope that reduces the gain,when Vbatt 3.3V, Please help provide the reference adjustment file of TAS2110 for battery, thank you.
Part Number: TAS2110 Hi Everyone,
Working on a PCB with the PN TAS2110 in parallel of the TAS2110 EVK as an example there are some differences on datasheet mentioning and maybe the I²C monitor on the software PPC.
Idle Channel Detection Switch
…
Other Parts Discussed in Thread: TAS2563 , TAS2110 We've designed and manufacture a device with TAS amplifier. In one revision we have TAS2110 while in different one it's TAS2563. How can I identify the amplifier by software?
Part Number: TAS2110 Hi TI experts,
I have came across a problem when using TAS2110 AMP IC for my design, which i am not able to obtain the output power (6.1W) as mentioned in the datasheet.
I only manage to get around 2.25W (3Vrms)
My measurement condition…
Part Number: TAS2563 Other Parts Discussed in Thread: TAS2110 , TAS2564 I've been using TAS2110 in my design for a while. It works fine. Last year it became unavailable, so my product upgraded to TAS2563, which seems to by pretty compatible with the former…