Part Number: TAS2110 Hello, I work on a custom board with TAS2110. Below is the schematic (please don't see on MPN IC1 on the schematic): /resized-image/__size/1333x768/__key/communityserver-discussions-components-files/6/TAS2110_5F00_schematic.png …
Part Number: TAS2110 Hi team,
Could you please check if TAS2110 I2C (SCL, SDA) is schmitt trigger input?
The I2C standard specifies the schmitt trigger.
Also, TAS2110 datasheet specifies the following hysteresis:
VIH(I2C): 0.7 × VDD (Min)
VIL(I2C)…
Part Number: TAS2110 I'm working on backporting the 5.8 mainline driver for the TAS2110 into my project. One thing I noticed is that minimum number of channels is specified as 2:
.name = "tas2562-amplifier",
.id = 0,
.playback = {
.stream_name …
Part Number: TAS2110 My customer is using this driver https://git.ti.com/cgit/tas256xsw-android/tas2562-android-driver/ and seeing an issue where sometimes when the I2S clocks are stopped and restarted quickly in succession, the chip is staying in its software…
Part Number: TAS2110
Hi,
My customer is evaluating the TAS2110 with the external PVDD.
It is described on the datasheet as below;
However, VBAT exceeds PVDD over 0.7V during a few ms on the power down sequence.
Should they improve this condition?
Best…
Part Number: TAS2110 Hi team, Your recommended EMI filters are 120Ω and 1nF for output in the datasheet. Is it possible to change to 220Ω to reduce noise? Is there any problem to change? Sincerely. Kengo.
Part Number: TAS2110
Hi,
My customer is evaluating the TAS2110.
When BST enabled, the output stops as below;
This phenomenon is improved by adding VBST pin capacitance.
Do you assume what is this caused by?
Though I'm requesting my customer to read…