Part Number: TAS2110 Other Parts Discussed in Thread: TCA9539 Hello team,
I found the TAS2110 D/S specifies the minimum I2C fall time (tf) as 20 + 0.1 x Cb ns at the fast mode.
I found my I2C signal from the SoC doesn't meet this specification.
Could…
Part Number: TAS2110 Hi team,
My customer is evaluating the TAS2110EVM.
The customer thinks that there is a writing error on the 8.5.45 BOOST_CFG4 in the d/s P.69.
1. The value at reset, when EVM is read, is 0x76h.
2. The customer thinks the Field is not…
Part Number: TAS2110 Other Parts Discussed in Thread: TAS2505 , TAS2552 , TLV320DAC3100 Hello expert,
May I have your recommendation for 2W/4ohm I2S audio amplifier solution? Customer will use 5V for power supply. Please kindly let us know if you have better…
Part Number: TAS2110 Hi,
Currently I don't have TAS2110EVM and I need to get a simple setup file for playing audio using I2S bus. Can I use PPC3 to generate a setup file without an EVM? For example if I set some options in "Device Control" does it transfer…
Part Number: TAS2110 Hi Team,
In the TAS2110 datasheet, the thermal information is shown for a YFP package. However, I believe the TAS2110 is in an RPP package. Would it be possible to please provide the thermal info for the RPP package?
Thank you!
J…
Part Number: TAS2110 Hello team,
My customer would like to quickly evaluate TAS2110. First, my customer would like to simply and quickly check the "sound" first.
But since customer doesn't have much time to evaluate, my customer doesn't have…
Part Number: TAS2110EVM Other Parts Discussed in Thread: TAS2110 I have obtained pure path console for the TAS2110 EVM but cannot seem to download any EVM apps , I can only install I2C master .
Am I missing a step here? do I have to request the EVM plug…
Part Number: TAS2110EVM Other Parts Discussed in Thread: TAS2110 Hello,
I recently applied for a development board for TAS2110.
When debugging with PPC3, I found that if the input volume is too high, the output will be intermittent, which is just like…
Part Number: TAS2110 Other Parts Discussed in Thread: TAS2557 Team,
What is the I2C voltage level? Is it limited by 1.8V VDD? My customer's system has 3.3V I2C only. If TAS2110 I2C is limited by 1.8V, can TAS2557 work with 3.3V level I2C? Thank? …