Part Number: TAS2110EVM Other Parts Discussed in Thread: TAS2110
Hi,
My customer is evaluating TAS2110 on the EVM and they can hear audible noise from a speaker.
The conditions are followings;
・Long speaker cable(the short cable is improved noise)
・Without…
Part Number: TAS2560EVM Other Parts Discussed in Thread: TAS2560 , TAS2110 Download unsuccessful
Hardware ID is incorrect
Audio sound card detected and unambiguous
Audio sound card sampling frequency is good
Unable to playback audio
* Console shows device…
Part Number: TAS2110EVM Other Parts Discussed in Thread: TAS2110 , Hi TI Team,
I am using the TAS2110 EVM module with the nRF52840 chip.
I am trying to provide external i2c signals from nRF52840 chip, as per TAS21110 EVM user guide
using the default address…
Part Number: LM386 Other Parts Discussed in Thread: LM380 , TAS2110 Hi team,
Could you give me comment on following customer question? The customer firstly selected LM386, but the increase of output power is needed based on proto type test result.
Q1.…
Part Number: TAS2110EVM Other Parts Discussed in Thread: TAS2110 Hello TI Team,
I am using the nrf52840 development kit to feed i2s signals to TAS2110 EVM externally.
I like to provide i2c signals also externally for other configurations of TAS2110 EVM…
Part Number: TAS2110 Hi TI experts,
Thanks for the supports...
We've encounter some issues of no sound output from TAS2110 just by power up-down the devices.
This symptom was occurred intermittently.
We've dump out the registry between OK and NG…
Part Number: TPA2011D1 Other Parts Discussed in Thread: TAS2110 When EN is set high, device starts cycling, with a large current spike on VDD every 100 msec. It looks like it's drawing high inrush current, then short circuit shutdown and auto-recovery…
Hi Wayne,
Let me ask a couple questions:
Are you able to configure the device by using tuning and audio processing panel, and playback audio through the EVM, even though there is error during system checks?
Do you need a standalone TAS2110 app due to…
Hi Ivan,
I found the problem. There is a wrong BCLK clock.
I Have :
BCLK = 48 KHz
WLKC = 48KHz
I think WLCK is OK but not BCLK. The tas2110 is a slave device or a master ?
I have to configure BCLK on the tas2110 (which register ?) or with the IMX processor…