Other Parts Discussed in Thread: TAS3204 Hey there,
Creating a board based on the EVM, with USB interface for programming - does the TAS automatically configure the usb host? Or do we need some special code in the eeprom attached to the USB to enable…
Other Parts Discussed in Thread: TAS3204 , TAS5630 Hello,
we are using the TAS3204 in our new CAM-474 Audio amplifier project right now.
I am looking for a level detector component to use with the pure path studio that clears a GPIO when a certain audio…
Other Parts Discussed in Thread: TAS3204 Dear ladies and gentleman,
I have a short question regarding the valid signals ranges for the analog inputs of a tas3204 DSP. Since the DSP is running from a single supply voltage I would have expected that the…
Other Parts Discussed in Thread: TAS3204 Hi,
I am trying to get the following scheme working in TAS3204:
TAS3204 has been configured to run in slave mode. I have generated the code (attached) using PurePath Studio GDE (version 1.88 build 5) and downloaded…
Hi Chia Cheng,
The TAS3204 that you refer to has no direct support although it is still active. I'm not able to help you determine if the TAS3204 is the best replacement for CM108B.
Other Parts Discussed in Thread: TAS3204
I now have the TAS3204 up and running on my own PWB using a PIC micro to control the run time properties of the DAP using the i2c bus. However, I am experiencing unpredictable and intermittent problems with the…
Other Parts Discussed in Thread: TAS3204 Hey there everyone.
ON the TAS3204 when GPIO1 is held low at startup, the system goes into passthrough mode - my question is does this include the analog paths? ADC and DAC?
Cheers
David.
Other Parts Discussed in Thread: TAS3202 , PCM3070 I just unpacked it and set it up. Only to find out today that it's discontinued. Love it when that happens. Life's cruel jokes...
If only TI made something else suitable.
Other Parts Discussed in Thread: TAS3204 , TAS3108 Hello
I want do download a configuration to the TAS3204 through I2C in slave mode. Does anybody know how the communication must look like?
I have the slave output file from pure path studio and don't…
Other Parts Discussed in Thread: TAS3204 Dear ladies and gentleman,
I'm trying for quiet a time now to get a TAS3204 DSP working and after some discarded pcb layouts I finally produced a layout with low noise and a working TAS3204. Or at least I believe…