I have a design that started producing audio at 1942 DSP words, but a tone generator set to 1kHz was producing 490Hz ... I had to go down to 1626 DSP words to get the right frequency out of it.
I hope that the DSP word count will be corrected in the…
Other Parts Discussed in Thread: TAS3204 Hi,
In my typical use of the TAS3204, I've never had a need to know what the TAS3204 will do if it doesn't have an external EEPROM; suddenly I have an application where I might need to know that. I don't have an…
Hey there,
Looking over the circuit for the TAS3204EVM, creating an application that only uses the analog in and outs, how much of that evm can be deleted?
I can understand needing the USB host adapter for programming etc - but is any of the digital…
Other Parts Discussed in Thread: TAS3204 I'm working on a project based on the TAS3204 DAP using Surepath Studio. I need an AGC function to boost low level signals using a relatively long decay time and cut high level signals with a fast attack time. Can…
Other Parts Discussed in Thread: TAS3204 , OPA1632 Hello TI community,
I'am new to the world of the TAS Audio DSPs and just finished my first board with the TAS3204. Now like almost always the problem is to get the chip running. The hardware is completed…
Other Parts Discussed in Thread: TAS3204 Hello,
how can i use the TAS3204 Mute-Pin. In the Datasheet i have found only this information:
Mute and power down functions have to be programmed in the EEPROM boot code. These are
general-purpose input…
Other Parts Discussed in Thread: TAS3204 There is a discrepancy between the I2C_addr.addr file generated by PurePath Studio and the TAS3204 data sheet. Here is a section from my I2C_addr.addr file:
Application: PurePath Studio Graphical Development…
This will probably be a stupid question, but could something similar to ALE be used to construct filter coeficient with the TAS3204?
It is a very convenient little program, I used it with TAS3004.
Thanks,
Mark
Dear Neil
I am faceing the same problem that want to download the program via the mcu(stm32f10x) 's I2C ,the TAS3204 I2C act as the slave
but my purepath studio version is 1.82 build 5
I can't find the "slave download" option !
…