Other Parts Discussed in Thread: TAS3308 I use PurePath Studio GDE V.1.8.2 to programm the TAS3308 EVM - Low Cost.
Firstly I like to loop the I2S input signal to the PWM outputs and the SPDIF Output. Just to test the device is running correctly. Unfortonally…
Other Parts Discussed in Thread: TAS3308 Hello,
I need more info on 'Scale' component under 'Basic DSP' in PurePath Studio for TAS3308. I am using PurePath 1.88 Build 5.
Following is the info available from PurePath documentation…
Hello.
I am trying to replace the EEPROM with MCU slave download for cost saving.
I have got the .cfg from PPS 188b3, 188b5 , edit it carefully and then download via I2C.
After downloading F/W , the status register shows 0x162 (D40 - D32),
D40 D39…
Other Parts Discussed in Thread: TAS5631 , TAS3308 , TAS5613 , TAS5086 Hello
I currently test a personal board who involve a tas3308 DSP for audio processing together with a tas5613 as power amplifier in a 2.1 configuration, actually everithing work fine…
Other Parts Discussed in Thread: TAS3308 Hi,
I have a very annoying problem with Purepath v1.88 build 3 (which I think is the latest for TAS3308?)
In one of my designs I am using several splitters (12) based on the component Split_TI_v2 and one of them…
Other Parts Discussed in Thread: TAS3308 Hello,
Probe Points GUI is able to collect data in real-time from TAS3308 and display the signal as a chart/graph. This data is collected at a maximum refresh rate of 15Hz. When I try to see a 1kHz signal, it…
Other Parts Discussed in Thread: TAS3308 Just started using Purepath Studio today to program a TAS3308. The issue I am having is when I set a biquad to be either high-pass or low-pass, 2nd order, variable Q. I use the Biquad GUI to to this and it appears…
Other Parts Discussed in Thread: TAS3308 Hi
I am having some problems in muting the TAS3308 with external HW control through the mute pin.
The description of the IIC mute control register 0x09 is indicating that the default value with mute(1:0) = 00…
Other Parts Discussed in Thread: TAS3308 Hello,TI!
I bought TAS3308 EVM. There was EEPROM 24LC512xxx by MICROCHIP.
I try to change EEPROM to AT24C64(my project is very small).
When i download code i see follow message:
----------------------------…
Other Parts Discussed in Thread: TAS3308 Hello, TI!
I have a two little questions:
1. TAS3308 are compatible with TAS3218 , in I2C commands ? 2. I can`t find initialization TAS3308. (Maybe exist official document). With best regards, Vladimir.