Other Parts Discussed in Thread: TAS3308 Hello, TI!
I`am trying to develop system on TAS3308 and can`t find complete pin description . Can you help me ?
With best regards, Vladimir.
Other Parts Discussed in Thread: TAS3308 Hi All,
I have built the TAS3308 LC EVM into a powered speaker and providing 5V to the EVM to power the board when the usb is not connected.
When the back is on the speaker it seems that after so long when everything…
Other Parts Discussed in Thread: TAS3308 , CC2530 Hello, TI!
I was looking TAS3308 datasheet, and found on page 4 (application information) two "VR_ANA2" pins and two "AVSS_PLL"pins. Is it right ?
With best regards, Vladimir.
Other Parts Discussed in Thread: TAS3308 , DIR9001 Hello, TI!
I using TAS3308 EVM. There is Optical Input(S/PDIF in I2S) on the board.
In User Guide speaks that 2-channels SPDIF receiver is present. But TAS3308 supported 6 synchronous I2S channels.
…
Other Parts Discussed in Thread: TAS3308 Hello, TI! I have`t PurePath Studio, may i configure (and start) TAS3308 with my MCU only ? Or i have to write micro program for 8051 core before and then send it to the chip and only after that i can configure…
Other Parts Discussed in Thread: TAS3308 Hello, Ti!
I want to use TAS3308. But i need equalizer (i need bass boost and other effects)
I think i have to:
1. Compile algorithms in PurePath Studio
2. Write compiled algorithms into EEPROM
3. Connect EEPROM…
Hi Drew,
Sorry for posting in the answered topic but I think it is suitable to post my question here
My customer is working on the same (not exactly) above design. We are looking for the I2C communication protocol so that the external MCU can send the…
Other Parts Discussed in Thread: TAS3308 Hi,
I am designing a 4 channel amplifier around the TAS3308 with digital input only. The boardspace is very tight so I would like to save as many components as possible so i would like to remove the analog supply…
Other Parts Discussed in Thread: TAS3308 Hello.
I use purepath studio GDE 1.82 build5 with TAS3308 EVM-LC.
When I change the delay Msecs Runtime property by PPS GDE properties tab, the i2c subaddress 200 (0xC8) has the sample size value.
But I try with…