Part Number: TAS5342 Other Parts Discussed in Thread: TAS5548 , TAS5142 , TAS5612LA , , TAS5614 Hi TI experts,
My customer want to design 8ch Audio system.
1. Is it possible to design with TAS5548 + TAS5342?
2. Could you provide the design guide document…
Part Number: TAS5342 Other Parts Discussed in Thread: TAS3251 , LMG1210 , TAS5558 , TAS5548 Hi,
Please recommend a PN to replace TAS5010 and TAS5342. These will be used in the new design of my customer. thanks.
Part Number: TAS5342 I am working on a design that only requires a 15V rail to hit my power targets. Disregarding the requirements of GVDD_X, and VDD (clearly stated in data sheet) is 15V at PVDD_X within the recommended operating limits? The data sheet…
Part Number: TAS5342A Other Parts Discussed in Thread: TAS5342 I'm using the TAS5342A in an amplifier design, and am designing a heatsink to connect to the top exposed pad with thermal grease in between. In looking for the proper standoff height for the…
Other Parts Discussed in Thread: TAS5342 , TAS5342A Hi,
I am using the TAS5342a in SE mode to amplify an analog PWM input. I am using only one of the four available channels. At the output of the TAS5342 I only get a DC voltage which is exactly the same…
Other Parts Discussed in Thread: TAS5352 we are plan to use TAS5352 in our design.
is we maintain separate AGND and DGND in our board?
Please advice
Thanks and regards,
Chandravel.
+919840383248
I using SE mode and 4 channels output from one power stage.And the performance is not bad.
but my system tas5342 is a bit hot.I also use TAS5508+TAS5342 which 5342 is not very hot.Is there anything specifical when using TAS3308+TAS5342?
HI
I'm using the GUI for the eval board TAS5342DVV6EVM version 4.0 RevA. I'm having issues with the volume control, it does not adjust. Nothing comes out until the input hits a certain level and I get max volume. The volume control seems to adjust…
Hi Robert,
thank you for providing these alternative devices. Indeed they look easier to implement. Unfortunately I fear 5.5V is too low (specifications aren't fixed, yet). The DRV595 is very expensive, thus not my favorite.
The device will be driven…