Other Parts Discussed in Thread: TAS5142 , TAS5342A ^ years ago we designed a new line of multi channel amplifiers using the TAS5142. At this moment the product is going through a major redesign. When I look at the product catalogue, it seems to me that…
Hi Steve,
I posted a new question titled as "TAS5342A driving 2.1 speaker". So far I got no response on it. I wonder if you are able to help. TAS5342A is used in another BT speaker project, to drive a 2.1 speaker. I would like to get some hints on how…
Other Parts Discussed in Thread: TAS5342 , TAS5342A Hi,
I am using the TAS5342a in SE mode to amplify an analog PWM input. I am using only one of the four available channels. At the output of the TAS5342 I only get a DC voltage which is exactly the same…
Other Parts Discussed in Thread: TAS5558 , TAS5624A , TAS5538 , TAS5352 , TAS5624 , TAS5768M , TAS5754M , TAS5352A , TAS5342A Dear Sirs,
My customer is using the TAS5558 + TA5624A. They consider TernaryModulation but do not be able to operate. Do TernaryModulation…
Hi, San,
Probably the easiest thing to do is to use an MSP430 to program the TAS5508C (I recommend you use it instead of the B which is NRND status).
Also, I suggest you TAS5342A or TAS5342LA as those parts are much newer.
For a reference, look at RDK…
Hi Don,
thanks for your reply! So the purpose of this delays is not what I thought.
Would be nice to let us know the optimal Inter Channel Delay values for the Digital Power Amplifier Stage TAS5342A which is on the Kit tas5342ddv6evm
- or to confirm…