Other Parts Discussed in Thread: TAS5352A , TAS5342LA Hi
We have question about the output of TAS5352A.
Could you review the following figures?
1. TAS5342LA
2. TAS5352A
We got these results in the same board. (It means TAS5342LA has been replaced with…
Other Parts Discussed in Thread: TAS5342LA Hi
We are looking for a digital amplifier meeting the following request.
Input: PWM
PVCC:12V
Output: 2ch BTL : 10W+10W RL= 6ohm, 1ch PBTL : 20W RL=6ohm
We consider TAS5342LA, but it seems to have much power…
Other Parts Discussed in Thread: TAS5342LA , TPA3140D2 , TPA3118D2 Hi
We are looking for the audio amplifier meeting following spec.
PWM input
2ch (BTL) : 10W/ch , 6ohm
1ch (PBTL) : 20W , 6ohm
Supply : 12V/3A
At first, we reviewed TAS5342LA but according…
Hi Matthew
Thank you for your reply.
Do you have a recommended solution instead of TAS5132?
For example, TAS5342LA can be used with BD modulation in PBTL/BTL?
BestRegards
Hello, Ying. The closest I can recommend is an open loop power stage amplifier, such as the TAS5342LA. The open loop response will offer a better gain at 40 kHz than our closed loop parts (which roll off quickly at 20 kHz), and you can design an output…
Hi, San,
Probably the easiest thing to do is to use an MSP430 to program the TAS5508C (I recommend you use it instead of the B which is NRND status).
Also, I suggest you TAS5342A or TAS5342LA as those parts are much newer.
For a reference, look at RDK…