Part Number: TAS5414B-Q1 Other Parts Discussed in Thread: TAS5414 Has it gotten too expensive to mold a simple dimple into a plastic IC package to denote pin #1? The TAS5414 data sheet says there is a laser burn mark on this part in the corner containing…
Part Number: TAS5414B-Q1 Hi,
Could you please share the information for "Output Power vs PVDD" with me ? My requirements are shown as below.
Case #1 - Configuration : BTL - Load Impedance : 4Ω - THD+N : < 1%
Case #2 - Configuration : BT…
Part Number: TAS5414B-Q1 Hi,
Is the master clock from 357kHz to 500kHz able to be applied to OSC_SYNC pin to synchronize 2 parts if I2C_ADDR pin is set to OSC SLAVE1/2/3 ?
Best regards, Kato
Part Number: TAS5414B-Q1 Other Parts Discussed in Thread: TAS5414 Dear Team,
do you have a graph that describes the derating of gain with temperature when any output channel is in thermal foldback?
Or any explanation what gain we shall expect at higher…
Part Number: TAS5414B-Q1 When the power is turned on, the inputs of the chip have a constant voltage of 4.4V independently or not. According to i2c:
step 1 I read registers 0x05 in response 0x0F I read registers 0x06 in response 0x00 I read the registers…
Other Parts Discussed in Thread: TAS5414B-Q1 , TAS5414C-Q1 Hello. This is Minsu Han.
I'm considering TAS5414B-Q1 for our applications.
We have to handle 2 Ohm speaker.
I have some question below items.
1) There are 4 output on TAS5414B. Can TAS5414B-…
Part Number: TAS5424B-Q1 Hi TI experts,
We used TAS5414B-Q1. we plan to change design to TAS5424B-Q1 due to L/T issue of TAS5414B-Q1.
If I connect INx_Mpin to GND, can I use TAS5424B-Q1 as a single-ended input?
Please check it.
Thank you.
Part Number: TAS6424L-Q1 Other Parts Discussed in Thread: TAS5414B-Q1 Hello team,
Our customer plan to use 2 units of TAS6424L-Q1.
Does this device have phase interleave function between 2 units?
In my memory, TAS5414B-Q1 had OSC_SYNC pin for avoiding…
Other Parts Discussed in Thread: TAS5414B-Q1 , TAS5414 Hello,
I work as design engineer in automotive industry. I used on my design IC TAS5414 with success. But In new revision (MK02) of PCB (in progress) I have to use TAS5414B-Q1. The layout is same as…
Other Parts Discussed in Thread: TAS5414C-Q1 , TAS5414B-Q1 Hi,
Could you please tell us whether we can use the gui of TAS5414C-Q1 as control software when evaluating TAS5414B-Q1? It seems that although we used it, it was not problem.
Best Regards, Kato