Other Parts Discussed in Thread: TAS5414B-Q1 , TAS5414 , TAS5414A , TAS5414C-Q1 Hi all,
Class D of AMP is a question about TAS5414B-Q1.
all the channels since mute I2C control data is got, Time until it carries out mute actually differs for every measurement…
Other Parts Discussed in Thread: TAS5414B-Q1 , TAS5630 , TAS5630B , TPA3116D2 Hello.
I'm an Electronic Engineer in a automotive speakers company and we are developing an amplifier that must have around 1 x 90 - 100 Wrms, with 14,4 V single power supply (DC…
Other Parts Discussed in Thread: TAS5414B-Q1 , TAS5611A Hi,
Would you perform the following evaluations?
My customer wants a result by this week.
-----------------------
<condition>
・PVcc=24V
・RL=4Ω
・BTL
・Input Wave = Square wave
・Output Wave…
Satoshi-san,
1. The TAS5414B-Q1 is available in the DKD package. There is no plan to release the TAS5414C in the DKD package.
2. There are minor software changes needed to go to the TAS5414B-Q1 device. It will work with your TAS5414A software, but you…
The input of the TAS5414B-Q1 is a high impedance input. A volume control can be easily placed on the input of the amplifier. The circuit to drive the volume control is not part of our amplifier and you must design it according to your system requirements…
Other Parts Discussed in Thread: TAS5414C , TAS5414C-Q1 , TAS5414B-Q1 Hi team,
I knwo already about TAS5414C version versus B version. TI recommends C version, however I should be B for PBTL.
C has register for PBTL. How about B? do I need any register…
Tiziano,
This device is derived from the TAS5414B-Q1 device. The datasheet appears to be needing some updating to remove all I2C information. Please disregard any mention of I2C and gain changing. All settings are fixed and one cannot change anything…
Other Parts Discussed in Thread: TAS5414C , TAS5414C-Q1 , TAS5414B-Q1 Have some questions regarding the TAS54x4 parts and documentation:
The 5414C datasheet mentions paralleling ch1&2 or ch3&4, but doesn't say anything about paralleling all channels.…
Other Parts Discussed in Thread: TAS5414A , TAS5414B-Q1 [ TAS5414A / B ] Replacement and Difference
Hi,
My customer has been using TAS5414A for past few years, and now they start to working on TAS5414B for new development. As first trial, they just replaced…
Tom,
I am not familiar with the output of the STA device, so I cannot recommend a detailed circuit. Generalizing, I would look a "cookbook" type low pass filter. Make sure the filter cutoff frequency of this PWM filter is lower than the the…