Part Number: TAS5414C Other Parts Discussed in Thread: TAS5414A , TAS6424 , TAS5414B-Q1 Please let me know about three points below for change TAS5414A to TAS5414C.
①Is there RTM schedule for TAS5414C's DKD (HSSOP) package?
Customer is very worry about…
Part Number: TAS5414C-Q1 Hi,
Could tell me the values of LC filters which you would recommend for 2ohm load impedance with BTL mode ?
Best regard, Kato
Other Parts Discussed in Thread: TAS5414C Hi,
I received questions about TAS5414C from a customer.
Q1. As shown in the table below, if we use an external oscillator with frequency 3.76Mhz to drive MASTER TAS5414C, what is the switching frequency of this…
Part Number: TAS5414C-Q1 Hi,
Could you please tell me the absolute maximum ratings for /FAULT pin which should be connected to 3V ~ 5.5V with the pull-up resistor ?
Best regards, Kato
Other Parts Discussed in Thread: TAS5414C Hi,
I received a question about TAS5414C from a customer. The question is as follows;
If customer have only one TAS5414C chip, can they use it as a Slave instead as a Master by connecting I2C_ADDR (pin 62) to D_BYP…
Other Parts Discussed in Thread: TAS5414C-Q1 Hi,
I have a question about TAS5414C-Q1,TAS5424C-Q1 datasheet. Q: Are the second rows of Table 17 - 23 respective reset (default) values?
Best regareds, Akio Ito
Other Parts Discussed in Thread: TAS5414 Hi.
Now we are trying to run TAS5414. I2C work works correctly.
Power up sequence:
1. STANDBY pin to 1
2. Wait 1 ms
3. Reading register 0x00. R0x00=0x00
4. Reading register 0x01. R0x01=0x00
Load diagnostic section…
Other Parts Discussed in Thread: TAS5414C-Q1 , TAS5414C Team,
I have a few questions about the TAS5414C-Q1 device when using the SYNC signal.
1. What would happen to the TAS device, while operating with a SYNC input, if we intermittently lost the SYNC…
Other Parts Discussed in Thread: TAS5414C-Q1 Hi, Team,
I have a question for TAS5414C-Q1.
What I want to know are bellows.
Is it OK to put 1uF cap on A_BYP and D_BYP? (I know it's not recommended by datasheet.)
-I guess the reason is related with…
Part Number: TAS5414CQ1PHDEVM Other Parts Discussed in Thread: TAS5414C , Hi,
I am trying to build the TAS5414C evaluation board, which I would also like to use as a normal amplifier. I found multiple schematics and documents related to this.
Option-1.…