Other Parts Discussed in Thread: TAS5508C , TAS5558 , TAS5548 Hi,
Context:
I'm writing a project candidate for Electronics students. The goal is to design and build an audio board for a full range 2.1 audio system (stereo + sub), which is completely …
Other Parts Discussed in Thread: TAS5508C , TAS5558 , TAS5548 , DRV632 Dear Sirs,
May I know what we need to config TAS5508C by I2C when sampling rate changed ?
Will TAS5508C automute output PWM during input MCLK/BCLK/FS dis-continue ?
Actually we hear pop…
Other Parts Discussed in Thread: TAS5518 , TAS5508C , TAS5518C I have used TAS5518. but 5518 is NRND.
so I try to change TAS5518 to TAS5508C.
what's the differences between TAS5518 and TAS5508C ?
Other Parts Discussed in Thread: TAS5508C , TAS5558 , TAS5548 , TAS5508 Dear Sir,
Is there EQ GUI tool can help TAS5508C EQ fine tune ?
ALE 5.2 generated EQ file format is not same as TAS5508C EVM tool.
Many thanks !
Other Parts Discussed in Thread: TAS5508C Dear Sir,
Would you give suggestion ?
Now we find the TAS5508C PWM output is nothing.
And the register 0x02 show 0xC0 .
Is there any initial setting is needed if my i2c source is same as TAS5508C default I2S format…
Other Parts Discussed in Thread: TAS5727 , TAS5508C , TAS5558 , TAS5548 Dear Sir,
How to add TAS5727 and TAS5508C EVM into control console ?
Many thanks !
Thank you Tuan, can you tell me is the TAS5508C a software drop in for the TAS5518. Can we use our existing TAS5518 commands on the TAS5508C ?
Also what are the advantages of the TAS5508C .
The TI reference design for the TAS5631DKD (slou275a.pdf) which I have been advised…
Other Parts Discussed in Thread: TAS5631B , TAS5508C , PCM4220 , TAS5558 , TAS5548 Hello,
thanks for reading my question. I'm actually planing a 2.1 High Quality Soundsystem with the follwoing Components:
PCM4220 AD Converter -> (I2S) -> TAS5508C -> (PWM…
Other Parts Discussed in Thread: TAS5508C , TAS5518 Hello!
In my device I use example schematics given in TAS5508C datasheet. On XTL_OUT there is a voltage varying from 1.8V down to 1V. On XTL_IN There is voltage from 0 to 200mV, and no resonant frequency…
Other Parts Discussed in Thread: TAS5508C , TAS5518C , TAS5518 , TAS5631 , TAS5508 Hello,
we are designing for a "audiophile" customer and used the evaluation module equipped with TAS5518C and TAS5631A with success for first prototype and for demonstration…