Other Parts Discussed in Thread: TAS5518C , TAS5508C , TAS5028 , TAS5558 I use TAS5518C with control by I2C and checking signal VALID
For beginning I switch on generator and I2S channel and clear reset of 5518c.
Because of VALID not appear, I read Error Status…
Other Parts Discussed in Thread: TAS5518C Is jitter presented on the MSCLK, BLCK, LRCLK directly coupled in the audio signal or is it resampled using the crystal clock of the TAS5518C ?
Or is it of any use to get the I2S signals arriving to the TAS5518C…
Other Parts Discussed in Thread: TAS5508C , TAS5518C , TAS5518 , TAS5631 , TAS5508 Hello,
we are designing for a "audiophile" customer and used the evaluation module equipped with TAS5518C and TAS5631A with success for first prototype and for demonstration…
Other Parts Discussed in Thread: TAS5518C Dear,
I'm writing controlling software for my TAS5518C plate amp, and have come to a hold. I need to know the sampling rate that is received by the TAS5518C, i thought i could read register 0X00 to do so. It…
Other Parts Discussed in Thread: TAS5518C I have designed a full digital amp using the TAS5518C.
When i power up the amplifier the output "Valid" of TAS5518C gives a spike which activates the output devices making "cracking" noise i the speakers.…
Other Parts Discussed in Thread: PLL1707 , TAS5518CTAS5518C has 2 clock inputs: master and bits. Jitter of bit clock or master clock is more influence on sound? Master clock I obtain from quartz generator on PLL1707 and bit clock from DSP. I can pass bit…
Other Parts Discussed in Thread: TAS5518C
How I can use two chips TAS5518C on one I2C bus?
It will work correctly if I make so:
SCL pass through "OR" element and second input of this element used as negative chip select
Other Parts Discussed in Thread: TAS5518 , CC8531 , TAS5518C I would like to ask regarding this PWM codec.
I need to use 300W amplifier by using TAS5631PHD evaluation module. As I look into Purepath wireless configurator, TAS5518 was available in device…