Part Number: TAS5558 Other Parts Discussed in Thread: TAS5624 Hello, i am searching for input usb board3 EVM. But i cannot find where i can to buy this EVM. Can tell my where to buy this board. Thanks.
Part Number: TAS5558 Other Parts Discussed in Thread: TAS5548 Hi Team,
I have 2 questions that need your help to clarify.
From below info in DS, does 44.1KHz supported besides 48- 96- 192-?
2. Is external crystal must have? Can the MCLK supply from…
Part Number: TAS5558 Other Parts Discussed in Thread: TAS5624 hi to all,
we are thinking of using the TAS5558 and TAS5624 in our new amplifier design. We are wondering if we could buffer the PWM output of the TAS5558 to achieve better SNR THD+N. Do you…
Part Number: TAS5558 Other Parts Discussed in Thread: TAS5624 Hi,
Im Planing to 2.1Channel using tas5558,For Sub-woofer connection need to use one TAS5624 or I can connect The LC filter directly to output of PWM signal
Other Parts Discussed in Thread: TAS5558 Dear Team
we are looking for a PA amplifier of 100W output.
we want a 100V line system , without output transformer, in class D configuration
Current class AB amplifier has bulky lamination transformer for making…
Part Number: TAS5558 Other Parts Discussed in Thread: CC2540 Hello Ti, is there any way to update biquads in a click-less manner yet? Your main competitor offers some shadow regs for that purpose aka safeload(in fact it is simply Fs synced buffer), your…
Part Number: TAS5558 Hi Team,
I see the datasheet, only PWM_5 & PWM_6 can be configured as Line in/out.
And also below block:
My question is:
1. Does only PWM_5&6 can be used as Line out?
2. How about other PWM like PWM 7, 8, can be used…
Part Number: TAS5558 Other Parts Discussed in Thread: TAS5624A Hello,
I have a design application using the TAS5558 with a TAS5624A amplifier with (2N) BTL and AD modulation. Regarding driving the differential PWM into a 8 inch backplane with opto-isolation…
Part Number: TAS5558 Hello
My customer will use TAS5558-TAS5142DKD for FY2018 product ( currently in ES situation).
Here customer had questions below.
Please advise.
Q1 Reg 0xDE bit D24
What is the difference between " Use Frequency Scaling"…