Other Parts Discussed in Thread: TAS5611 , LM2755 I purchased a pre-made board using the TAS5611 chip with the view to integrate them into a product design, however when I input voltages above 16 (up to 31v), I get a constant high pitched squeal come through…
Other Parts Discussed in Thread: TAS5611 , TAS5611A , TAS5613A Hi,
Could you please tell us the difference between TAS5611 and TAS5611A?
Best Regards, Kato
Other Parts Discussed in Thread: TAS5611 , TAS5612LA , TAS5622A , TAS5611A Hello,
I have designed a plateform based on the TAS5611 amplifier chip.
My plateform is done to explore the multiple configurations available from this chip (BTL, PBTL) ; one of our…
Other Parts Discussed in Thread: TAS5611 Hello
regarding the TAS5611, I would like to use in single end mode (not in BTL mode like the confif of the demo boad).
Have you the value in dB regarding the PSRR when using this amplifier in single mode (4 HP…
I need to use TAS5611 with a single ended audio source.
What if I don't use the OpAmp stage and connect L_IN_N / R_IN_N to GND through a capacitor and use L_IN_P / R_IN_P for the audio input ?
I will only have half of the input signal magnitude, that…
Other Parts Discussed in Thread: TAS5611 Dear TI support,
I have a small 2.1 channel Home Theater (HTIB), that uses two TAS5611 chips. One for the front channels and the other for the sub. They work in master/slave mode that is the front amp is the master…
Other Parts Discussed in Thread: TAS5611A Hi all,
is it possible to use TAS5611A in PBTL configuration and AD mode ? I am using the EVM and I note that when configured for PBTL it selects BD mode. Is it just because the implemented output filter is not…
Other Parts Discussed in Thread: TAS5611 , TAS5612 , OMAP-L137 Hi,
I used the analog input power amplifier TAS5611 building a amplifier and it worked very well. We want to changed it to digital input TAS5612. I read the functional block diagram of TAS5612…
Other Parts Discussed in Thread: TAS5611 Hi,
I designed a Power Amplifier which used TAS5611 and it works very well. The bulk capacitor that I used is 1000uF, because both the EVM and Schematic of datasheet use 1000uF capacitor. In my case, the input…