Other Parts Discussed in Thread: TAS5611 , TAS5611A Hi.
I have problem with different power consumption on TAS5611 (TAS5611A). Power consumption change up to 1W with different IC on the same design.
Ir-camera show a great difference temperature on TAS5611…
Other Parts Discussed in Thread: TAS5611 Hi All,
We are interested in TAS5611,13 125W sterreo, it will be good if TI have power supply module or solution to supply TAS5611PHD2EVM as well.
MD
Other Parts Discussed in Thread: TAS5611 Hi,
I designed a power amplifier using TAS5611, and used another DSP to control it. It is recommended to hold pin /reset low in document. In our design, we need to turn on/off the PA frequently, so how long should…
Part Number: TAS5611A Other Parts Discussed in Thread: TAS5611 We are using the TAS5611A (X2 to drive a dual voice coil driver, 2ohms per coil) & we have based the design on TI’s Typical Differential (2N) PBTL application with BD Modulation filters (also…
Other Parts Discussed in Thread: TAS5611A , TAS5611 Hello, I am researching the TAS5611A and would like to know if I can DC couple the audio inputs (pins 4,5,10,11) using VI_CM (pin 6) as a reference.
Basically, does the device have bandwidth to DC without…
Other Parts Discussed in Thread: TAS5611A , TAS5611 , TAS5630B , TAS5613A What happens when TAS5611A is driven to it's extends and at some frequencies the load impedance drops below 3 Ohms while no Schottky diodes are present from OUT_x to GND?
Can the…
Other Parts Discussed in Thread: TAS5613 , TAS5613A , TAS5611A , TAS5611 Hi,
Could you please tell us the difference between TAS5613 and TAS5613A?
Best Regards, Kato
Do you have any recommandation about the possibility of using your closed loop references for 20KHz to 30KHz range which is quite close of audio range?
TAS5611/13 for example ?
Other Parts Discussed in Thread: TAS3204 , TAS5611 Dear Suzan,
I have a noise problem using the TAS3204:
In order to get a hight output from the TAS5611 I have to amplify the signal coming from the TAS3204EVM by 4 giving me a unacceptable high noise level…
Other Parts Discussed in Thread: TAS5611 hi
can i get circuit gerber(orcad)files for IC Tas5611 in which were given in the Data sheet and EVM board document . I am working for acoustic signal amplifier design for underwater communication. If u provide…