Hi Trey,
You had a nice ideea to use a Bluetooth audio link with your amplifier :)
I am building an amplifier using TAS5611. Can you please suggest a heatsink to be used, like the one you have on the board presented on Youtube ?
Thank you.
Other Parts Discussed in Thread: TAS5611 hi
I want to know power amplifer IC's number detail which will support frequency ranges of 5khz to 60khz ( and 20 w to 80 W). Most of the data sheet (from TI) says Amplifer supports up 20khz only.
what…
Other Parts Discussed in Thread: TAS3204 , TAS5611 , TAS5630 Hello,
We are using the TAS3204 together with a TAS5611 and we get a audible noiselevel over the speakers.
If I connect the inputs of the TAS5611 to ground it is quiet.
If I measure the output…
Other Parts Discussed in Thread: TAS5611 All,
we are interested in TAS5611, 13, it will be good if TI have power supply module or solution to use for 120W stereo. Do TI have such power supply solution.
MD
Other Parts Discussed in Thread: TAS5611A , TAS5611 , TAS5630 Hi,
anybody knows which is the threshold level of the CLIP warning signal from TAS5611A ? I did non find the value on datasheet, but perhaps I missed it.
Thanks in advance,
Enrico
Pierre, we actually have almost completed developing off-the-shelf inductors for TAS5630, TAS5631 and the rest of their family (TAS5611/2/3/4). I am checking with the vendor now to try to confirm that you could use that source. I will let you know ASAP…
Other Parts Discussed in Thread: TAS5611 , TPA3106D1 I have a customer with an application where the TPA3106 is not good enough.
He is looking for a class-D amp that is capable of ultrasonic tones (> 90 khz). Therefore the PWM clock must be 450 khz or…
Tyler, I will check about THD.
TAS5614 is NOT NRND!
TAS5615 and TAS5616 (analog and PWM inputs) are NRND. They were simply not in demand.
TAS5611/12/13/14 will stay in our catalog for a long time.
Regards,
Steve.
Hi, Gordon,
We do not recommend using the TAS5630 below 25V PVDD.
TAS5611 and TAS5613 are rated for lower PVDD operation. Please look at those to see if they will fit your needs.
-d2