Hi, Ken,
Almost all of us were out of the office...
Plus, you already answered your own question! I like customers like you!!!
You got it --> AD is req'd for SE operation.
The only analog parts we have that use AD are TPA312x family.
All the…
Thanks for that, I think on rev 1 I may risk a device and try not fitting filter or bst caps; I have also added 0R links near device to isolate tracks should I need to add BST caps.
According to spec, when switching each 1/2 bridge consumes 10mA gate…
Hi, Frank,
The TAS5611/13 are PWM input power stages. The current regulation will be dependent on your loop; our chip just takes the input PWM signal, and replicates it on the outputs. We do have feedback to correct for changes in the power supply voltage…
Other Parts Discussed in Thread: TAS5630 For the TAS5630, 5613, 5611....
Are the READY and CLIP output characteristics the same as the SD and OTW characteristics?
That is 26K pull up to 3.3V?
Other Parts Discussed in Thread: TAS5613 , TAS5630 Normal
0
I am debugging a 5613-prototype card, not the TAS5613
evaluation card. When power is on and
reset is off, the amplifier is in a state where the CLIP signal is always on –
even when…
Other Parts Discussed in Thread: TAS5613 I want to drive the TAS5613 with a stereo single ended source.
1. How do I connect the two single ended channel outputs to the TAS5613 differential inputs (and what mode should I use)?
2. One of the Modes (100…