Other Parts Discussed in Thread: TAS5613 , TAS5630 , TPA3123D2EVM , TAS5611A , TAS5615 , PCM1808 , TAS5086
The TAS5613 and TAS5630 are capable of delivering considerable power for a distributed 25 VAC audio system. Are these good candidates for achieving a…
Other Parts Discussed in Thread: TAS5613 , TPA3100D2 , TAS5613A Hi All,
We're designing a power output stage with the TAS5613. We've built a prototype board basing on the schematics of the TAS5613 evaluation board but i cannot find the toroidal inductor…
Other Parts Discussed in Thread: TAS5613 Hi,
I've earmarked the TAS5613 in stereo BTL mode for an aviation project. The only problem is that the qualification requirements includes operation at 85degrees Celsius ambient, while the TAS5613 is only rated…
Other Parts Discussed in Thread: TAS5613 Hi,
I'm designing 3x TAS5613 in a 6-channel application, powered with a 500W DC-DC half-brick supply (Synqor IQ24 series). Trouble is, the supply has a maximum stable load capacitance limit of 1000uF, and with…
Other Parts Discussed in Thread: TAS3103 , TAS3204 , TAS5613
ll
Hello
I am an embedded systems and power electronics engineer.
I am also and avid AV enthusiast and hobbyist
But hands on experience in audio is limited to only about five projects
I…
Other Parts Discussed in Thread: TAS5613 When the TAS5613 is first turned on (with reset low), the ready LED is solid for a few seconds and then it starts to blink.
What does the blinking mean?
Thanks..
Other Parts Discussed in Thread: TAS5613
I am testing a 5613 design and I am finding that given the
same level input: The output from the
5613 evaluation card is greater than the output from our own designed card.
One of the differences…
Other Parts Discussed in Thread: TAS5613 , TAS5613A dear Ti support engr,
i want to know from the basic apps diagram for driving a single speaker in BTL mode if the inputs must be driven in opposite phase...
Other Parts Discussed in Thread: TAS5613 Hello,
I am designing an amplifier around the TAS5613 IC in BTL using BD modulation, and have a question about selection of the output inductor. The inductor specified in the reference design is a Toko C3B-A0336…
Part Number: TAS5630B Other Parts Discussed in Thread: TAS5613 , TAS5630 Hi,
We have designed a range of amplifiers using the TAS5630B,TAS5613 and TPA3118 , during production we found that some amplifiers that use the TAS5630B chip overheats even without…