Other Parts Discussed in Thread: TAS5613 , TPA3116D2 , TPA3116D2-Q1 Hi,
I'm curious as to how the TPA3251D2 handles clipping. Another device (too small for use in this project, but a device I like very much) the TPA3116D2 uses a "compressor" style of "clipping…
Other Parts Discussed in Thread: TAS5613 , TPA3116D2 , TPA3118D2 , TPA3123D2 , TAS5630B , TAS5613A hi,
we are looking to run the following chips(TPA3118,3116 & TAS5613,5630) in single ended mode for a couple of quad channel amplifier.We would like to know the…
Other Parts Discussed in Thread: TPA711 , TAS5630 , TAS5615 , TAS5613 Class AB amplifier efficiency in SE configuration
Q: Class AB amplifier efficiency in SE configuration
A customer wants to use a TPA711 in SE mode to drive a 15 Ohm speaker. Could you provide…
Hello Dapkus,
Thanks for the reply.
We have used TAS5613 in our previous product. In the datasheet of TAS5613 the theta JC is 3.2 C/W.
TAS5630B output wattage is higher than TAS5613 so this question raised.
Regards,
Sreekanth
I wonder if the inductors are saturating (they do have a pretty steep sat curve). What is the output current, the Rocp resistor value, PVDD voltage, resistive load used (impedance), TAS5630 or TAS5613 used?
reg,
Paul.
Don:
Thanks for your response. It was helpful.
I have been doing a comparison of the TAS5613 and the TAS5630. Our target for delivered power is 2 x 60W @24 VAC. Both data sheets indicate that the TAS5613 is more efficient with these output parameters…
Other Parts Discussed in Thread: TAS5613 , TAS5614A Hello,
I'm searching for the package PHD S-PQFP-G64 for eagle. I can't find it in any library.
Please help me!
Other Parts Discussed in Thread: TAS5613 , TAS5611
Youtube Video:
http://youtu.be/9X-E9GXSX0c
The Bluetooth Audio Amplifier Boosterpack has many uses and has a wide target audience. The original project idea was to give tubers a way to make their own DIY…
Bruce, use the source ground as one side of each differential input to TAS5613. Connect each differential input between source ground and source Left or Right output. Remember, though, that during turn-on you will have to delay enabling TAS5613 until your…
Other Parts Discussed in Thread: TAS5613 , TAS5630 , TAS5611 , TAS5631 , TAS5614 Hi,
I'm using the TAS5630DKD with PSU rails at 40VDC. Power requirements are low at 90W/ch in 4ohms.
Implementation is very similar to the evaluation board, but due
to…