Other Parts Discussed in Thread: TAS5631 , TAS3308 , TAS5613 , TAS5086 Hello
I currently test a personal board who involve a tas3308 DSP for audio processing together with a tas5613 as power amplifier in a 2.1 configuration, actually everithing work fine…
Other Parts Discussed in Thread: TAS5613 Hi to all
We maid power amp by using TPA 3123D2. And it is found to be working good .now we are planning to make on sub amp (TPA 3106D1, TAS5613)
maha
Other Parts Discussed in Thread: TAS5613 , TAS5630 Normal
0
I am debugging a 5613-prototype card, not the TAS5613
evaluation card. When power is on and
reset is off, the amplifier is in a state where the CLIP signal is always on –
even when…
Other Parts Discussed in Thread: TAS5615 , TAS5613 , TAS5630 Hi, on page 25 of the TAS5615 datasheet there is a recommended reference PCB layout. Can you supply the BOM for this board and, in particular, the manufacturer and part number of the recommended…
Tomasz, this is good news. Thank you for letting me know. I am very pleased that you were able to work this out.
I believe the source of output noise is the input stage in both TAS5630 and TAS5613. Input stage noise performance was chosen to provide…
Hi, Gordon,
We do not recommend using the TAS5630 below 25V PVDD.
TAS5611 and TAS5613 are rated for lower PVDD operation. Please look at those to see if they will fit your needs.
-d2
Other Parts Discussed in Thread: TAS5613 , TPA3100D2 I have been using the TAS5613PHD2EVM evaluation card and it has been working great in our application. I just noticed that it always operates in BD mode. And it doesn't look like I can test AD mode to…
Hi Don,
Thanks for you reply. I followed this start-up procedure. The issue is that how long it will take between step(2) Apply VDD,GVDD and PVDD and step (3) Release /RESET. We used the DSP to control this start-procedure, so we need to set all of…
Other Parts Discussed in Thread: TAS5630 For the TAS5630, 5613, 5611....
Are the READY and CLIP output characteristics the same as the SD and OTW characteristics?
That is 26K pull up to 3.3V?