Hi Don,
thnx for the quick reply.
We use 48V as power bus voltage....which is too high for TAS5614 and 5624. ( if the datasheet is correct)
The options that are left are the TAS5631 and the TAS5162 which are capable of operating on 48V.
I wanted to use…
Tomasz
Thank you for the nice words on the tpa3116.
Have you looked at using lower impedance woofers? like a 2.5R - then a PBTL connected TPA3116D2 willl do 100W, and the benefit is that you can use a single 24V voltage rail for both the woofer and mid…
Other Parts Discussed in Thread: TAS5518 , TAS5614 TAS5518 can regulate volume with modulation of power supply voltage of output stage. It is very good. But I read datasheet on TAS5614 recomendate voltage supply between 18 and 36 V. It is only 6 dB of volume…
Other Parts Discussed in Thread: TAS5614 , TAS5615 , TAS5611 , TAS5614A I don't see any THD data/graphs in the TAS5612 datasheet when it is operating in Single Ended mode. I am investigating using this chip to tri-amp a powered speaker and I would like…
Other Parts Discussed in Thread: TAS5518 , TAS5614A , TAS5631 , TAS5614 , TAS5508C , TAS5518C State:
TAS5518 & TAS5614A at 192 or 176.4 kHz. All biquads switched off. DRC switchted off. Louness switched off. Only amplification control is used.
I want…
Pierre, BTW, Coilcraft are also in final review of the data sheet for MA5172-AE, identical to the inductor we have been using in TAS5631, TAS5611, TAS5612, TAS5613 and TAS5614 EVMs.
This is a 10uH toroid similar to MA5173-AE, also with Isat >20A, high linearity…