Part Number: TAS5622A Other Parts Discussed in Thread: TAS5342LA Hi Team,
For the same 1 watt output condition, the input PWM level is different,
is the circuit of the two devices the same?
are there any differences in the datasheets of the two devices…
Part Number: TAS5622A Hi Team,
My Monitor Speakers cannot pass the EMC test because the TAS5622A outputs 147.92MHZ is too high, please suggest the inductance value and capacitor specification.
Part Number: TAS5622A Hi Team,
If I change the input voltage of the tweeter to 12V, The input voltage of the subwoofer is 24V, Is there a problem with the circuit?
Part Number: TAS5622A Hi Team,
I measured about 32.5mA with no signal standby mode, It is twice as large as the specification of 12mA, Is this normal please?
Part Number: TAS5622A Other Parts Discussed in Thread: TAS5624 currently my TAS5624 idle PVDD current is around 140mA and the data sheet stated only 15mA during 50% duty cycle.
my current config is 2x SE and 1x BTL.
PVDD: 37V
Any setting that will cause…
Part Number: TAS5622A Other Parts Discussed in Thread: TAS5624A , , TAS5558 We are looking at TAS5622a or TAS5624A in PBTL configuration but we don't have the THD+N graph for 8Ohm...can you please share it ?
Part Number: TAS5622A Other Parts Discussed in Thread: TAS5538 , TAS5624ADDVEVM Hi team,
The customer is using TAS5622-TAS5624DDVEVM. The GUI for the EVM is TAS5538_GUI.
But there is no the User's Guide for TAS5538_GUI software. So the customer does not…
Other Parts Discussed in Thread: TPA2008D2 , TAS5622A , TAS5611A Dear sir,
for tas5622A amplifier ic requires an PWM input signal. is it possible to use tpa2008d2 as an preamplifier. please replay to me
thanks
kiran
Part Number: TAS5622A Other Parts Discussed in Thread: TAS5558 , Hi e2e,
One of my customer is trying to use our TAS5622+TAS5558 preceded by a PCM185 in an industrial power amp. They need to use an audio transformer at the amplifier output to match the…
Part Number: TPA5051EVM Other Parts Discussed in Thread: TAS5622A , TAS5614 , TAS5624A I received a tpa5051evm board. The pdf document mentioned a "TI input-usb board". Please tell me how to get the "TI input usb board".