Part Number: TAS5630 I am using the TSA5630 in ptbl mode with a subwoofer. I am using a 48 volt battery which runs at 53volts max. I completely unpluged the input signal but it still runs hot to the touch. And with a small input signal it wil overheat…
Hi Jesse,
Thanks for your reply.
I will check the PCN document with the link you commented on.
BTW, Could you please provide additional answers to the customer's inquiries below?
Q1) Is the TAS5630 B PHDR a good replacement?
Q3) Could you please provide…
Part Number: TAS5630 Hello TI team,
I'm going to design simple subwoofer amplifier, based on TAS5630B in PBTL mode.
The main idea of the design to keep main TAS5630 board in vertical position, where the rest of components, like main power supply,…
Part Number: TAS5630 Other Parts Discussed in Thread: DRV135
Hello,
I have creating custom board for TAS5630, size 10x10cm. Most critical are paths for PVDD and OUT_x.
Can you verify attached picture and provide feedback?
As input I will use DRV135…
Part Number: TAS5630 Hello,
In studying SLOU293C document, I cannot find the PCB/ Gerber files that I cannot do the further testing. Could you provide me with the related files for me to produce a test sample?
Best regards,
Louie
Part Number: TAS5630 Hi
I've used for 2 days Satisfactorily, the TAS5630 STEREO AMPLIFIER, made of SANWU CHINA, Applied 38 Volt DC, but now it gone to STANDBY MODE Permanently and not pulling out from it and not working, all Parameters, ie. Volt, Resistance…
Part Number: TAS5630 Other Parts Discussed in Thread: TPA3255 , Hi Team,
A customer wants to know the major differences between TAS5630 and TPA3255 and what makes the big difference in the price.
Regards,
Danilo
Part Number: TAS5630 We use TAS5630 chip made a 2.1 power amplifier board. After connecting the sound source, power amplifier and 2.1 speakers, there is no sound in the speaker every time when it is turned on. We must extract the speaker once in the power…
Part Number: TPA3255 Other Parts Discussed in Thread: TAS5630 , TAS5630B Hello All,
The datasheet recommended design and EVM schematic for both the TPA3255 and TAS5630 show a 100 ohm resistor in series with the INPUT_X pins of the IC. In looking through…
Part Number: TAS5630B Other Parts Discussed in Thread: TAS5630 Dear all, Please help me.
I make TAS5630 PCB. It good sound. After 3 hours of checked sound.
It have 4ohm speaker.
I have not turned off the power.
I don't give input, Only have white noise…