Other Parts Discussed in Thread: TAS5630 , TAS5630B Hi,
we are encountering failure of the TAS5630 while taking out 230 +230W @ 4E on a 52VDC rail . The amplifier works properly till it encounters Over temperature protection ..for the first 2-3 cycles it…
Other Parts Discussed in Thread: TAS5630 Hi
We are Planning To Design Isolated Power Supply for TAS5630 about 500-600W
hence We Referred " 600-W, Isolated PFC Power Supply for AVR Amplifiers Based on the TAS5630 and TAS563 " Design
we Think It…
Other Parts Discussed in Thread: TAS5630 , TAS5630B Hi All,
I have a customer who is using TAS5630, could you please help review the schematic as attached ? Thanks a lot for your help !
Best regards
William
Hi Ervin
we cannot say which one is much more suitable for Bass Guitar Amp.
considering power and THD, tpa3255 seems much better than tas5630.
I am not sure which amplifier less than 100w is more suitable for Guitar amp, but i think maybe you can consider…
Other Parts Discussed in Thread: TAS5630 , TAS5630B Hi! I have 4 TAS5630 synchronized together. They works in BTL Mode.
PVDD supply: 1000 VA toroidal transformer, 45VDC.
GVDD and VDD: a smaller transformer, 12VDC,
I have a soft start circuit for toroidal…
Other Parts Discussed in Thread: TAS5630 , TAS5630B I'm running a TAS5630 at PVDD=51V PBTL into 2 ohms.
The chart from the user guide slau287a indicates that 500W PVDD=50V THD soud be ~1%. In order to provide a little more margin I'm running at 51V.…
Hi Maciek
Please confirm, with 0.4V amplitude signal, do you mean the signal been sent into OPA1632 or is it the input level for TAS5630?
Can you test directly at the input port of TAS5630, what is the peak value of the sinewave signal?