Part Number: TAS5634 Other Parts Discussed in Thread: TAS5631 , Hi Team,
For 200WX2/4Ohm , TAS5634 can work continuous 180 seconds on BTL mode, How about TAS5631? which solution would working longer( same heatsink size and same power supply) ? any difference…
Part Number: TAS5634 Other Parts Discussed in Thread: TAS5631 , Hi Team,
My customer is evaluating TI's Power Stage amplifier, just want to know the difference between TAS5634 and TAS5631.
Thanks and regards
Part Number: TAS5631 hi,
TAS5631DKDR This material we have experienced several burning phenomena in use, after which 5pcs samples were sent to CECC for failure analysis.
Our doubts are:
1. The analysis report pointed out that there are stratifications…
Part Number: TAS5631 Hi All
My clients use TAS5631 in their project. They test TAS5631 under the condition of 4Ω load,the supply voltage is 35V,work frequency is 100Hz,the output power is about 120W. After the test starts 15 seconds, the thermal protection…
Part Number: TAS5631 Dears
we have the TAS5631DKD2EVM, but we can't find the file of 'Configuration (1.00).cfg' mentioned in TAS5631DKD2EVM user's guide , Would you pls supply it ? thx
TAS5631DKD2EVM.PDF
Other Parts Discussed in Thread: TAS5631 , TAS5631B Dear forum,
Does anybody know if there are any actual differences between TAS5631 and TAS5631B devices?
I can only see changes in the datasheets concearning the way the devices are specified.
Geert
BD Modulation will reduce your output ripple amplitude, but you also can stay at AD because 1.2V with 384 khz is in a good range i think.
For a switch to BD you have to change the I2C settings, and you should also change the Mode Pins on the TAS5631. …
Other Parts Discussed in Thread: TAS5631 Hi All,
Please let me know that whether i can get the source code for TAS5631 GUI or else application for linux platform.
Thanks and regards,
ATUL KUMAR SINGH
Other Parts Discussed in Thread: TAS5631 , TAS5630 Hello, I have to design A 2 * 300 W digital Power amplifier, want to use "A 600 - W, Isolated PFC Power Supply for AVR Amplifiers -based on TAS5630 and TAS5631" of the Power Supply scheme. In order…
Hi,
I noticed that even if I pull the /RESET low, /SD stays low.
I read in datasheet on page 23:
"Asserting the reset input low removes any fault information to be signaled on the SD output, i.e., SD is forced high."
Does it mean, there is something…