Other Parts Discussed in Thread: TAS5631 Hi
I'm working on a custom board who use a TAS5631,DKD package in 2*SE + 1*BTL configuration, the problem is that the TAS5631 seem to be never ready, whatever i do, the SD and OTW remain always hight.
My…
Other Parts Discussed in Thread: TAS5631 , TAS3308 Hello
I'm currently testing a personal board with a TAS3308 + TAS5631 in a 2.1 configuration, during a test the TAS5631 was destroy and i don't know why.
When the problem apear only the central…
Other Parts Discussed in Thread: TAS5631 Hello TI Community.
I have a question about the TAS5631 digital audio amplifiers :
Is there any delay between the lower level PWM input signal and the higher level PWM output signal ?
On the way from the PWM …
Other Parts Discussed in Thread: TAS5631 , TAS5630 , TAS5162 Hi,
Currently we are evaluating a new design incorporating the TAS5631.
We use the DKD version, 2 x BTL at 48V. AD modulation scheme
At 3.5 Ohms load, some 2dB before clipping, spikes apear…
Other Parts Discussed in Thread: TAS5631 , TAS3308 , TAS5342 , TAS5162 Hi
I plan to use the TAS5631 drived by a TAS3308 DSP in a single ended configuration, the TAS3308 have a special startup sequence for SE configuration called mid-z, i want to know if…
Other Parts Discussed in Thread: TAS5630 Hi,
The reference design SLOU293A "A 600W, Universal Input, Isolated PFC Power Supply for AVR Amplifiers Based on the TAS5630/5631" found at http://focus.ti.com/lit/ug/slou293a/slou293a.pdf mentions…
Other Parts Discussed in Thread: TAS5631 Hello guys,
Does anyone knows why the TAS5631 in PBTL mode is not specified for 8 ohm load impedance ?
Is there something 'hidden' ? This PBTL mode works with 8 ohm impedance or not ?
Thanks
Domini…
Other Parts Discussed in Thread: TAS5631 , TAS3308 , TAS5613 , TAS5086 Hello
I currently test a personal board who involve a tas3308 DSP for audio processing together with a tas5613 as power amplifier in a 2.1 configuration, actually everithing work fine…
Other Parts Discussed in Thread: TAS5630 , TAS5631 , TAS5518 I have looked over the TAS5630/31 data sheets for any information on low frequency reponse to no avail. On the analog input version TAS5630 you can do an input stage which blocks DC and for the PWM…
The suggestions made were quite helpful in eliminating the TAS5631 part as the immediate cause of the output disturbance. The various delays in the serial data stream made it difficult to trigger and capture the fact that the data stream actually was…