Part Number: TAS5634 Hi,
we observe EMI diificultys in mode 011 (2xBTL, AD modulation).
Slew rate at PWM C+D is >20ns, with minimal overshoot. Disconnecting doesn't affect EMI measuremt.
Slew rate at PWM A+B is <10ns, with massive overshoot. Disconnecting…
Part Number: TAS5634 Other Parts Discussed in Thread: TAS5614LA , TAS5614 Hello Expert, I'd like to confirm about whether we can use this device with case that GVDD voltage is higher than PVDD voltage. As far as my understanding, there isn't any limitation…
Part Number: TAS5634 Hello,
I am looking to implement a 250W RMS in to 4Ω in PBTL. In the TAS5634 data sheet the Typical PBTL config (Fig 29) shows the use of 4 inductors, one each for OUTA,B,C,D. Is this required to prevent over current issues, and…
Other Parts Discussed in Thread: TAS5634 Dear TI
Can I use the TAS5634 for BTL output mode, the power is 2*100W, can the load be two 4 ohm speakers? Because I see the specification BTL mode is only 8 ohms and 6 ohms.
Part Number: TAS5634 Hi Sirs, Do we have a power stage to support load conditions of 400W, 1%THD+N at 2ohm PBTL and 200W, 1% THD+N at 4ohm BTL? The TAS5634 can achieve 400W at 3ohm PBTL and 200W at 6ohm BTL which cannot meet customer's requirements. Thank…
Part Number: TAS5634 Other Parts Discussed in Thread: TAS5558 , Hello,
on the ti website, in the parameters section, a Sampling Rate (max) is reported.
What is releated to this parameter?
The suggested I2S to PWM (TAS5558) works with a 192kHz…
Hi Adam,
Please refer to attachment for the construction and inductor's specs.
Construction & Specs.xlsx
"Higher load of 5 ohm requires PVDD to be lowered. With 30k ROC, PVDD in 5 ohm case should be max 53V, at 27k ROC, up to 56.5V PVDD can be used…
Part Number: TAS5634 Other Parts Discussed in Thread: TAS5538 , PUREPATHCONSOLE
HI TI,
For TAS 5534 output channel configuration, I want to select channel 3, channel 4 to Front Left , Front Right speaker and channel 1 to subwoofer.
I have reference…
Part Number: TAS5634 Other Parts Discussed in Thread: TAS3251 Hi, I'm pretty sure this is a stupid question (because of EMi and high freq...), but I dare asking. Can there be a short (10-15cm) wire connection between an audio PWM controller (like TAS5508…
Hi Kwan,
The firmware for PMP20873 hardware is for demo purpose only and not available for public yet . Please check back later on the product folder for updates . Thanks, Sanatan