Other Parts Discussed in Thread: TAS5706B Good morning.
I'm using a TAS5706B in a dual mono configuration, so I have two IC for a stereo amplifier.
I use channel A and B in BTL mode.
First question:
can I miss to connect the components to channel C…
Other Parts Discussed in Thread: TAS5706B , TAS5706 , TAS5103 I'm using TAS5706B in a dual mono configuration, so I use only one channel in BTL configuration with two IC.
Microcontroller update the DAP configuration even during music play, I can change…
Other Parts Discussed in Thread: TAS5706B Hello,
We are using TAS5706B in 2.0xBTL mode on 4 ohm loads. On our ptototype, we are facing some problems at high level, which was not noticed on EVM board. Supplied with 22V, we reached 13Vrms with the EVM boards…
Other Parts Discussed in Thread: TAS5706B Is it possible to connect the TAS5706B to an OMAP processor? If so, has anyone had experience getting them to talk?
Other Parts Discussed in Thread: TAS5706B Hi
I have try the setup (2-ch single-end + 1 channel Bridge) for TAS5706B.
However, the 1 channel bridge should be L+R channel.
I have tried the setup based on the "TAS5705-L+R-sum implemetation" but it do…
Other Parts Discussed in Thread: TAS5706B , TAS5706A Since the TAS5706B is not available within a reasonable lead time(20weeks). Can the TAS5706A be substituted for the TAS5706B in a single ended application? What is different about the TAS5706B that allows…
Other Parts Discussed in Thread: TAS5706B Question: I am using the TAS5706B in my solution and it is working well. It does exhibit a small pop at power-up. In my system the PVDD comes on before any of the other power supplies (IE: DVDD). Can you suggest…
Other Parts Discussed in Thread: TAS5103 , TAS5706B I want to drive a little 4Ohm Woofer with the TAS5103. It is recommended to use either SE or PBTL config for 4Ohm loads (datasheet P. 7).
For more power I'd like to use PBTL mode, but there are no further…
Other Parts Discussed in Thread: TAS5760MD , TAS5706B , TAS5756M , TAS5760M , PCM1792A , TPA3132D2 , PCM5122 , TAS5754M Hello,
We are currently designing an audio streamer that must meet the following requirements: -stereo 2x 20W output on 8 or 4 ohms speake…