Other Parts Discussed in Thread: TAS5707 , TAS5711 art Number: TAS5707
Hi Team,
customer would like reduce choke/ inductance such as below fig ,could you help to check this settting. ,is that ok or nO?
TAS5707 ,Mono CkT with 4 choke
BR,
SHH
Part Number: TAS5707 Other Parts Discussed in Thread: TAS5711 Hi,
My customer is exploring to use TAS5707 in mono mode using only one of the available channel. However, we aren't sure if this configuration may induce any issue since the device is design…
Part Number: TAS5707 Other Parts Discussed in Thread: TAS5711 , TAS5709 , Hi, Team
My customer is using TAS5707/TAS5709/TAS5711 in their TV board product. They find there is a circuit in red circle which is use to anti-pop noise in their old schematic. They…
Part Number: TAS5707TAS5707 has no PWM output.
And current measure results of our board are below: 1. I2C comunication is OK; 2. Falut pin is always high;
3.source file: wav 24bit 48KHz;
4. MCLK=BCLK: 3.06MHz, LRCLK 48KHz;
5. AVDD 3.28V,PVDD 12.2V;
Is there…
Part Number: TAS5707 Other Parts Discussed in Thread: TAS5711 , TAS5731M , TLV320ADC3101 Dear All,
project:loudspeaker box
The box need take reference signal horn to do echo cancellation. Our hardware only collected data of a trumpet.Speakers (R…
Part Number: TAS5707 we use 5707 as amplifier when the DRC is turned off, the sound is too small, According to datasheet we can know if we want to set DRC threshold need to fill in several values, how can these values fill in the threshold can increase…
Part Number: TAS5707
Hello everybody,
i'm trying to setup my TAS5707 board without the PSIA interface board from the eval kit.
By now, i'm struggeling to initialise the TAS5707 from an AVR via I2C. The I2C is tested working, so sending bytes should…
Part Number: TAS5707 Other Parts Discussed in Thread: TAS5733 Hi Sir
Where can I find the thermal parameter of TAS5707 ??
I cannot find it in spec.
thanks for reply.
BR
Yimin
Part Number: TAS5707 Other Parts Discussed in Thread: TAS5733 Hello Audio Folks, my customer is using TAS5707. They have found a pop noise in playing a sound and stop it. They say it is OK after removing the added EQ and change the SSTIMER reg 0x1A from…
Other Parts Discussed in Thread: TAS5707 , TAS5756M , TAS5754M Error issue: when use 48kHz or 12kHz sample rate,the TAS5707 frequently mute the audio output with timelong 17ms per 80ms; when use 32kHz or 16kHz sample rate, this issue also happen ,but the time…