Other Parts Discussed in Thread: TAS5707 , TAS5708 Dear Sir
Good days,
We have as below two questions need check with you.
1.Due to power saving, we use remote control for sleeping control switch.
PVDD(24V)/DVDD(3.3V) use PMOSFET to do switch, when our product…
Other Parts Discussed in Thread: TAS5707 I am debuging new design with TAS5707 + ARM M4 + MEMS microphone.
I cannot get any sound from TAS5707.
I am running on fs=16kHz, BCLK=768kHz MCLK=6,144MHz
I am using MCU crystal which is 8MHz so the master clock…
Other Parts Discussed in Thread: TAS5709 , TAS5707 Dear Sir,
Is there any easy way to set bass boost of TAS5707 just like the TAS5709 bass boost on/off control ?
Is there any example of how the set the EQ of TAS5707 to do bass boost?
Hi Leon,
I found that TAS5707 supports 16K sampling rate but it is no longer recommended for new designs. Do you have a good part number recommendation?
Other Parts Discussed in Thread: TAS5707 Hi,
I refer to TAS5707 EVM.
1). May I know what is the function of R9 resistor 22.1kohm (P22.1KHCT) which is connected to pin 7 (OC_ADJ- analog overcurrent protection line) of TAS5707?
2). How does this pin…
Part Number: TAS5733L Other Parts Discussed in Thread: TAS5731
hi,
We have a project based on the amlogic platform。and PA use tas5733L.now there are accompaniments but no vocals when playing music.
Register initialization code is as follows.
What should…
Part Number: TAS5711 Other Parts Discussed in Thread: TAS5707 Tool/software: TI C/C++ Compiler hi Team:
I designed TAS5711 Connect with MCU,could you pls help to support sample program?
Hi Shawn
The TAS5707 can report UV error. Why the TAS5751 can not report the error? Is there any difference between the two device?
Thanks and best regards,
Ella
Hi Sebastien,
PDN can be driven to High after AVDD/DVDD is stable, so there is no issue in the datasheet description. Please refer to this post: e2e.ti.com/.../422604 It's for TAS5707, but also applies to TAS5733L.
Best regards,
Shawn Zheng