Part Number: TAS5753MD Other Parts Discussed in Thread: , TAS5707 I failed to notice the 100us requirement to ramp PVDD after AVDD/DVDD. What happens if these come up at the same time?
Other Parts Discussed in Thread: TAS5707 , TAS5707A , TAS5731 Hello,
i'm using the TAS5707 Evaluation Module. Was working without any problems so far.
Since yesterday i get an error in the output window of the GDE (using TAS5707 GUI v2.0.1 Build 14 Rev…
Hi KH,
How much is the RMS voltage on the output pins? It's supposed to be PVDD/2 if there is no input signal or the device is in the MUTE state. Did you measure the waveform on the output pins, it should be 50% duty-cycle square waveform after initialization…
Hi Mike,
Congrutulation! When the inut signal amplitude is low, you need to enlarge the volume to achieve a larger output power. About the volume setting, please refer to the Table 12 in the TAS5707 datasheet. The PWM output is supposed to be 384kHz or…
Part Number: TAS5707A Other Parts Discussed in Thread: TAS5707 Hi
Briefly, we think there is the following power sequence for TAS5707.
Power Up: AVDD/DVDD = 3.3V applied first, then PVDD=20V applied Power Down:PVDD powered down, then AVDD/DVDD powered…
Other Parts Discussed in Thread: TAS5707 , TAS5707EVM , TAS5751M , TAS5733L Hello,
I just bought a TAS5707 Evaluation Module and wanted to install the TAS570x GDE. I didn't find a download link from TI.
In the forum i found the Software-Version 7608.TAS570X_v2…
Other Parts Discussed in Thread: TAS5711 , TAS5707 Hello Audio Folks, do we have a pin to pin test report for TAS5711? A customer is asking for this.
Regards,
Kes
Hi Diego,
Yes, LC filter is populated. I can get the same phenomenon on the TAS5733L EVM.
I have tested several other amplifiers with the same configuration. Only TAS5733L can't work. Others such as TPA3110, TAS5707 and TAS5711 is still working even…
Other Parts Discussed in Thread: TPA3144D2 , TAS5711 , TAS5707 Hi everyone!
I have designed my own Bluetooth speakers using the TPA3144D2. I just tested it with 2 6W/8 Ohm/ 8kHz Speakers and it sounds great! But I want to improve the sound quality just…