Hello Allex,
Thanks for the feedback, We'll check this and see the way to include this in next document revisions.
About the GUI failure, when installing the software, TAS5707_08 tab should appear by default, if not, you may be able to open it from…
Hi Hasebe-san,
As you said, I believe that TAS5731M will set the power stage to Hi-Z if detecting the overcurrent since it does not have a cycle-by-cycle current-limiting function like TAS5707.
So, please refer to "9.3.4.1 Overcurrent (OC) Protection…
hi,Don Dapkus
thank you for your concern and your help
i will wait for your colleague's answer until next week.
before this project,i have used TAS5707 and TAS5708 in my hardware for my project of lab of xidian university
TAS5713 has a lot of differences…
Other Parts Discussed in Thread: TAS5707 Hi,
Could you please tell us whether the PWM modulation method is the full digital pwm modulation or the analog pwm modulation with DAC regarding the digital to PWM conversion block? In addition, could you please…
Other Parts Discussed in Thread: TAS5707 , TAS5707A Hello,
Can I use the MC57xxPSIA to communicate with the TAS5707EVM2 mounted with a TAS5707A instead of TAS5707?
My question is where do I select the TAS5707A (different I2C address) in TAS570X GUI?
…
Other Parts Discussed in Thread: TAS5707 I'm designing a board with the TAS5707, and I'm trying to figure out the better modulation method to use. Looking through the datasheet and the LC filter recommendations, it seems to me that BD is generally…
Other Parts Discussed in Thread: TAS5707A , TAS5707 , TAS5717 Hello,
I have TAS5707A EVM (with MC57xxPSIA board), for which I2C device address is 0x3A sa per datasheet.
While using TAS570x GDE software tool, choosing TAS5707_8, issues device address 0x36…
I understand why 0x0F replaced by 0x03 in register X27 - X35. it is because access to unused bits.
However, I still do not understand why register X50 vaule changed to 0x0F 0x70 0x80 0x10. this is initialization value. but the datasheet shown the default…
Hello Don Dapkus;
Thank you for suggestion TAS5760MD
Please elaborate details / advice regarding TAS5707 series application of HP ~50mw Head Phone
The product already in production however this is an attempt to offer an add on hardware solution using
a…