Other Parts Discussed in Thread: TAS5713 , TAS5708 , TAS5707 hi,
I've read datasheet and user's guide of TAS5713,and here is my confusion:how to balance two band DRC in TAS5713?
we have used TAS5707 and TAS5708 in our hardware board from our project…
hi,Don Dapkus
thank you for your concern and your help
i will wait for your colleague's answer until next week.
before this project,i have used TAS5707 and TAS5708 in my hardware for my project of lab of xidian university
TAS5713 has a lot of differences…
Hi, Jay,
TAS5706/16 & TAS5708 are the only closed-loop options with MCLK=SCLK support, and even this is valid only for 44.1K/48K Fs clock (64*Fs SCLK, MCLK).
I would recommend TAS5708 as it is our second-generation device. TAS5706/16 are first generation…
Hi Bogey,
1. Are you using the EVM? The GUI software with the EVM also controls the TAS5707 via I2C. The GUI is downloadable from http://www.ti.com/tool/tas5707evm .
2. If you have looking for low power, the TAS5708 is close in functionality and has…
Hi Ali,
Unfortunately, we don't have anything pin-to-pin compatable. However, the TAS5708 is very close in functionality/pinout with the same package (while being closed-looped).
Regards,
~John
Other Parts Discussed in Thread: PCM1808 , TAS5708 Hi,
I have purchased the TAS5708EVM which comes with MC57xxPSIA to evaluate TAS5708 + PCM1808 combination.
The analog input on MC57xxPSIA which is through PCM1808 generates high levels of background noise…
Other Parts Discussed in Thread: PCM3070 , TAS5708 Hi,
I'm working on a design that couples together PCM3070 and TAS5708. I'm utilizing both I2S and line outs of PCM3070.
I'm using the 8x4x framework
FS = 48Khz
CODEC_CLKIN = 86.016Mhz
NADC, NDAC…
Other Parts Discussed in Thread: TAS5717 , CC8520 , TAS5710 , TAS5708 , TAS5727 , TAS5713 , TAS5518 The 8520 configuring software with the tas5717 selected generates this line of code
w 36 1B 00 # set factory trim.
this is not consistent with the address of…
Other Parts Discussed in Thread: TLV320AIC3204 , TAS5708 , TAS5713 , TLV320AIC3254 , TAS5710
Hi all,
there is now an update available for the PurePath Wireless Configurator software. Enhancements in PPWC version
1.0.1 includes support for new external…