Other Parts Discussed in Thread: TAS5713 Hi Team,
Customer Amtran is asking for the TAS5713 EQ adjustment.
They use the TAS5713 in PBTL woofer mode. An the BiquadControl is enable.
Amtran adjust the EQ (either BQ1 or BQ2), but there is no change on the…
Other Parts Discussed in Thread: TAS5713 Hi Team,
Our customer uses the TAS5713 GUI. The GUI can set the setting and get the output waveform. But we can not mute the TAS5713 through control GUI.
Did you have latest TAS5713 GUI for customer? Thanks!
…
Other Parts Discussed in Thread: TAS5713PHPEVM , TAS5713 Hello
My client is evaluating TAS5713; TAS5713PHPEVM.
He Connect USB, using TAS5713_GUI_v3.3 build 11 and just shutdown/mute button removed then master vol=0dB.
He did not get same cross talk value…
Other Parts Discussed in Thread: TAS5713 , TAS5708 , TAS5707 I'm from china xidian university ,and i'm going to use TAS5713 in my hardware from the project in my lab
here is my problem
when i read the TAS5713 datasheet ,the register 0x56 and 0x57…
Other Parts Discussed in Thread: TAS5727 , TAS5713 Hi
I was wondering if there is a power sequence for the DVDD/PVDD on the TAS5713 or the TAS5727. We are thinking of using the PVDD (18V) rail as the source of our DVDD(3.3V) thus making the PVDD active…
Other Parts Discussed in Thread: TAS5713 Hi
I want to use the Equalizers in the chip for tone control of an Active speaker in real time. I can simulate my needs in the GUI but I don't see what register I need to change when I change the Gain on each filter…
Other Parts Discussed in Thread: TAS5713 Hi
Where can I find the formula to calculate the B-quads registers. As I see from the Evaluation Board and the Gui that for every change in the Gain or the Frequency of a filter I need to recalculate the values…
Other Parts Discussed in Thread: TAS5715 , TAS5713 Hi,
I have been looking at the TAS5713 and comparing it to the TAS5715. In terms of output power they seem very similar. Are there any output power advantages to using the TAS5715?
Thank you
Other Parts Discussed in Thread: TAS5717 , TAS5716 , TAS5713 , TAS5719 Hello,
We are designing a board with several amplifiers chips. Currently we are using TAS5716 in SE mode and we'd like to move to BTL mode but the problem is our speakers are 4ohm so we…
Hi Eli,
The statement -- "The clock section uses MCLK or the internal oscillator clock (when MCLK is unstable, out of range, or absent) to produce the internal clock (DCLK) running at 512 time the PWM switching frequency.".......
......is trying…