Other Parts Discussed in Thread: TAS5717 Hi,
I am using TAS5717 to drive 2 W speakers. I will supplying 24V as PVDD. Is it safer to drive 2W speaker using TAS5717 with 24V?
Regards
Charles
Other Parts Discussed in Thread: TAS5717 Hello Folks,
We are planning to use TAS5717 in our design. I have a few doubts regarding this power amplifier. I am driving 4 ohms 2 W speaker using this PA. Will it work in that if I provide 5V to PVDD supply? …
Other Parts Discussed in Thread: TAS5717 Hi,
Could you please tell us how to output the internal /FAULT signal(D1 bit of 0x02) to A_SEL or HP_SD pin if possible ?
Is our understanding correct although we believe that D1 bit and D0 bit for the 0x05 register…
Other Parts Discussed in Thread: TAS5717 , TAS5719 , TAS5727 any negative consequences in using the TAS5717 or TAS5719 as a mono amp in parallel mode? I will be driving a 6ohm impedance. I read in another post that it was "ok" as long as the wiring is done…
Hi John
thank you very much for your study and analysis.
for this chip is too old, i also not very familiar with it. but according to my search, i think your understanding should be right.
please refer below 2 e2e, their comment seems very close to yours…
Hi,
We are considering to decrease the external components since we don't use the headphone amplifier. Could you please give us your advice about unnecessary external components ? For example, - Not apply the power supply for HPVDD - Not use the decoupling…
Other Parts Discussed in Thread: TAS5717 Hi,
I had setup the TAS5717 evm and GUI. I am able to read and write to the TAS5717 registers through GUI. I fed the EVM with audio from mobile using stereo to mono splitter. I am using 3W 4 ohm speaker. I am not…
Hi,
We are considering to decrease the external components since we would like to use the left channel only for the BTL mode. Could you please give us your advice about unnecessary external components ? For example, - Not use the external LC filter and…
Other Parts Discussed in Thread: TAS5717 Hey guys, I have some trouble getting the TAS5717 running:
The input signal is a 16 Bit-I2S, 44.1kHz, a simple 440Hz sine.
The first question, are these the minimal settings and right order to possibly get a sound…
Hello,
is there any possibility to mix left and rigth channel to a mono signal after application of the volume control block? So the goal is to combine/mix one mono signal maintaining its constant volume level (such as a signal tone) with another mono…