Other Parts Discussed in Thread: TAS5717 , TAS5717EVM I am trying to characterize TAS5717 for a new design with TAS5717EVM board.
My setup is
LIN = 1VRMS
RIN = 1VRMS
JP4 is selected for ADC
VIN = +5V
PVCC = +20V
I can connect with TASGDE and read register…
Other Parts Discussed in Thread: TAS5717 Hi
I'm having trouble starting up the TAS5717 on a new design. I used the EVAL schematic as a reference when creating my design but I can not get the chip to start up. Should I hear some level of pop when the…
Part Number: TAS5719 Other Parts Discussed in Thread: TAS5717 Hi Team,
My customer is using TAS5719 for 8W 6 ohms design. The output filter is 22uH + 1uF in BTL mode. Fs either 44.1KHz or 48KHz.
They are measuring the SPL output from our TAS5719 using…
Other Parts Discussed in Thread: TAS5717 , TAS5704 Dear Sir
Good days,
May we double confirm with you if TAS5717 can work without connect I2C?(I think Tas5717 can't work)
My customer use Quick filter IC that I2S output and will no use MCU.
Best regards…
Other Parts Discussed in Thread: TAS5717 , TAS5717EVM i'm having some trouble bringing up a tas5717. I currently have the circut below wired up to a pure path audio EB.
3.3v (vdd) is supplied from the EB and the 5v is supplied by a benchtop supply. …
Part Number: TAS5782M Hi Team,
Our customer used the TAS5782M as the core amplifier in their consumer audio hardware device but they noticed that there are audible clicks when changing EQ settings during the playback. According to our customer,
We successfully…
Other Parts Discussed in Thread: TAS5717 Hi,
I am new to audio signal processing so please forgive me if the answers are too obvious.
I am trying to figure out how to setup TAS5717 DRC to properly limit the audio output with desired compression ratio.
In…
Other Parts Discussed in Thread: TAS5717 Hi.
I purchsed TAS5717 evalkit a week ago.
But I have some troubles about this eval kit.
I am using digital audio (coaxial) and I connected two set of 8ohm speaker. (OUT1/2 - Left, OUT3/4 - Right)
I just execute…