Other Parts Discussed in Thread: TAS5717 Hello,
Via I2C, I am setting the registers in the TAS5717 (slave) from a LM3S9B96 (master) micro-controller.
These are the values I am setting:
(the first hex number is the register I am writing to, and all the…
Other Parts Discussed in Thread: TAS5717 , CC8520 , TAS5710 , TAS5708 , TAS5727 , TAS5713 , TAS5518 The 8520 configuring software with the tas5717 selected generates this line of code
w 36 1B 00 # set factory trim.
this is not consistent with the address of…
Other Parts Discussed in Thread: TAS5717 Dear Mr. Dapkus,
I posted about TAS5717 evalkit experiment a week ago. And I have been waiting your reply.
Could you look into the problem?
Best regards,
Byungkeun Lee.
Other Parts Discussed in Thread: TAS5717 , TAS5717EVM I've wired up a circut containing a 5717 to the mc57xxPISA that came with my tas5717 evk. I can connect over i2c and register 0x00 reads as 0x6c.
I set the ch1 vol 1 and 2 to 1.0 and set the master…
Other Parts Discussed in Thread: TAS5717 Hello there,
I'm working on setting a TAS5717 amplifier to have a specific sound profile, and going through the config file generated by the GUI (TAS57XX GDE), it sends 8 bytes of data to registers that can only…
Other Parts Discussed in Thread: TAS5727 , TAS5717 , TAS5721 , TAS5707A Hi
I see in the parametrics sheet on the TI website that the TAS5727 can be run in single ended mode, but I found nothing in the datasheet on that mode. Is this correct?
Also, is it possible…
Other Parts Discussed in Thread: TAS5717 I am trying to play audio files to a TAS5717 using I2S 16bit data. at 32000 Hz.
The TAS5717 is reporting a LRCLK error.
To play an audio file:
Sample Rate Generator is setup
Frams sync (LRCLK) and bit clock is…
Other Parts Discussed in Thread: TAS5717 , TAS5716 , TAS5713 , TAS5719 Hello,
We are designing a board with several amplifiers chips. Currently we are using TAS5716 in SE mode and we'd like to move to BTL mode but the problem is our speakers are 4ohm so we…
Hi,
The equation for the release (decay) time constant listed in TAS57xx Dynamic Range Control guide (SLOA148, p3) doesn't match the value shown in TAS57xx GDE software (TAS57XX ver 3.2 build 7) . could you tell me the correct equation for converting…
Other Parts Discussed in Thread: TAS5717 Hi-
I'm looking for a little more information on the Osc Trim register-
***********************
OSCILLATOR TRIM REGISTER (0x1B) The TAS5717/9 PWM processor contains an internal oscillator to support autodetect…