Part Number: TAS5717 My set up is as below:
Vin and GND- 5V input
PVCC and GND 9V input, shutdown off, mute off and volume turned to MAX.
Lin- 1Vpp sine wave from Function Generator, JP2 shorted, JP4 connected to ADC , USB powered from PC, Speaker of…
Part Number: TAS5719 Other Parts Discussed in Thread: TAS5717 , Hi Sirs, The TAS5717/TAS5719's MCLk and BCLK input must be aligned with each other as we know. Would you pls advise if we can make them align on falling edge as the picture below? Thank you…
Part Number: TAS5717 Other Parts Discussed in Thread: TAS5727 I2S typically only requires 3 signals.... SCK, SD and WS.
How do I configure the TAS5717 to function with nothing attached to the MCLK pin? What are the limitations in this mode?
Hi Pascal,
The register 0x3d, 0x44, 0x45 are not availabe on TAS5717. The document SLOA148 doesn't apply for TAS5717. On some devices, like TAS5711, these registers are all available. And actually DRC in TAS5717 is not as complex/powerful as TAS5711.…
Part Number: TAS5717EVM Other Parts Discussed in Thread: TAS5717 Tool/software: WEBENCH® Design Tools When we use the TAS5717/19EVM board connecting with mother board MC57xxPSIA, After connected, un-check shutdown and mute we can't read data in I2C…
Other Parts Discussed in Thread: TAS5717 I have the eval module outputting audio, both with audio input and wiring in I2S into the pins.
Both ways, the output appears saturated, squared off, though it is at low levels (<1Vpp).
The 2 channels (C,D…
Other Parts Discussed in Thread: TAS5717 Hi Team,
The customer is using TAS5717. The audio signal is input by I2S. He needs to achieved this function. The sound can be output from a 2*10W speaker when
the headphone is not inserted. The sound can be output from…
TAS5717 data sheet verbiage states that the 7-bit I2C address is 0x54. This is incorrect. The 7-bit address is 0x2A. The R/W bit is not included in a 7-bit address.