Hi,
Could you please tell us the transition time for the output FETs if a short circuit on the output is shorted to GND and is removed as below ?
Q1. the transition time from the normal mode to Hi-Z for the output FETs when the output is shorted to G…
Other Parts Discussed in Thread: TAS5717 , TAS5731 , TAS5713 , TAS5719 , TAS5731M Hi,
We believe that the power on/off sequence which you recommend for TAS5717 and TAS5719 is same with TAS5713 and TAS5731.
Is our understanding correct ?
Best regards,
…
Other Parts Discussed in Thread: TAS5717 Hi,
Could you please tell us the recovery time from the overcurrent protection if a short circuit on the output is removed ? Moreover, when is /FAULT pin asserted to low although the overcurrent response time is…
Hi,
Could you please tell us the value of the internal pull-up/down resistors regarding those pins of /PDN, /RESET/ and so on ?
Is our understanding correct although we guess that it is more than 48kΩ(3.6V/75uA), referring to the input current for the…
Other Parts Discussed in Thread: TAS5717 Dear Team:
Our customer new design used TAAS5717 to be mono output, but input is stereo.
We would like to use mixer function to achieve it by TAS5717, but datasheet only showed register 0x51, 0x52 brief description…
Other Parts Discussed in Thread: TAS5717 I made a original board with TAS5717.
Headphones always have white noise whatever I2S data is all 0.
Speakers don't have noise.
Output waves of Headphones have spike noise about 500kHz period.
When the signal…
Other Parts Discussed in Thread: TAS5717 , PUREPATHCONSOLE Dear Sirs
I use TAS5717 and develop the EQ function of TAS5717 in one project.
In another project, I use TAS5756. It's all new design.
May I transplant the EQ function setting from TAS5717 to TAS5756…
Other Parts Discussed in Thread: TAS5717 Hi everyone!
I need more described information about TAS5717 Data Sheet.
page1 DESCROPTION:
" Oversampling combined with a fourth-order noise shaper provides a flat noise floor and excellent dynamic range from…
Other Parts Discussed in Thread: TAS5717 Hi everyone !
I need information about TAS5717.
I have two quetion.
Question1:
We can setting the MCLK=SCLK.
Is there anything "reduce of performance".
i.e.)
-LRCLK:48kHz Fs
-SCLK:Fs×64=3.072MHz …
Other Parts Discussed in Thread: TAS5717 Hi,
I am using TAS5717 Audio amplifier in my application. I want to use 3 W speaker and i have option to provide either 5V or 24V to PVDD. Please help me to configure DRC settings for PVDD 5V and 24V.
Regards …