Hi Nethra,
This feature should work normally on MC57xxPSIA + TAS5717EVM. Please refer to the jumpers setting on MC57xxPSIA board for input configuration at e2e.ti.com/.../3529.mc57xpsia-board-input-configuration .
Could you please confirm the analog signal…
Hi, Safeer,
Ternary mode uses the same same ICD settings as BD modulation. The amplifier should not have issues when using it in BD or AD modes, the noise you heard and the inductor heating is an abnormal behavior. Do you have a output capture, as well…
Other Parts Discussed in Thread: TAS5717 , TAS5717EVM Hi,
Now my work is to write sw to drive the speaker, we use the TAS5717 driven by iMX6(freescale ARM CPU) to drive the speaker.
I'm new to the digital audio stuff, and I've already read the datasheet…
Hi Charles,
I would like to check the humming noise is caused by TAS5717 and its related circuit.
Is it possible to fly audio source(output of codec) to TAS5717EVM?
Regards,
Will
Other Parts Discussed in Thread: TAS5717 , TAS5717EVM Hi,all
Please let me ask a question about TAS5717.
When customer make Audio source to TAS5717 via Optical ,audible noise is outputed from AMP output while no sound.
Could you teach me a coping strategy…
Other Parts Discussed in Thread: TAS5717EVM Hello,
I've been trying to run the GDE for our TAS5717EVM. My Laptop is running Windows 7 64-bit.
After a fresh install, when I start the GDE, I always see an error:
Requested component (BQ3) not found
…
Other Parts Discussed in Thread: TAS5717 , TAS5717EVM I am trying to characterize TAS5717 for a new design with TAS5717EVM board.
My setup is
LIN = 1VRMS
RIN = 1VRMS
JP4 is selected for ADC
VIN = +5V
PVCC = +20V
I can connect with TASGDE and read register…
Hi Alex,
What I2C slave-address are you using? Do you see I2C transaction with a nack on the scope?
I've viewed the signal on the scope. Starting from the start condition the bytes are 010101101
The address in the datasheet is listed as either 0x54…
Other Parts Discussed in Thread: TAS5707EVM , TAS5717EVM , TAS5731 Is the MC57xxPSIA included with the TAS5717EVM? Product Folder page for the TAS5710EVM does state the MC57xxPSIA is included, as well as the TAS5707EVM PF page, but the TAS5717EVM PF Page…
We have a new board with no more edits on it. hpvss and hpvdd connected, HP_SD and A_SEL connected to ground and vcc through 15k resistors.The new board is exhibiting the same symptoms as before. When I bring it out of shutdown in the GUI I hear a pop but…