Hi Brandon,
There are 3 kinds of input are available: analog, OPTO/RCA and I2S. Please refer to the detailed explanation in this link
Please make sure to apply 5V power supply on VIN connector. Please read the TAS5719 EVM user's guide and follow the procedure…
Hello Mickey! Alex can help you further with your question, but the TAS5717 is just a different power level version of the TAS5719 and does not support SE. Could TAS5721 or TAS5731M work? Thanks, Jeff
Other Parts Discussed in Thread: TAS5717 , TAS5719 , TAS5727 any negative consequences in using the TAS5717 or TAS5719 as a mono amp in parallel mode? I will be driving a 6ohm impedance. I read in another post that it was "ok" as long as the wiring is done…
Hi Xiaoling,
Please take a look at the TAS5719 device. It is an I2S input 15W stereo class-D amplifier, with integrated HP/Line-driver.
http://www.ti.com/product/tas5719
-Ravi
Adrian,
7485.TAS5719_Measure.zip
At your Request, Ravi and I measured TAS5719 today. And will measure TAS5713 tommorrow.
If you need additional information, or have questions. plz let us know.
thanks.
- Patrick Lee
Part Number: TAS5717 Other Parts Discussed in Thread: TAS5782M Hello,
I need to implement a parametric equalizer using the TAS5717 biquad cofficients. That means I need to calculate the biquads on the fly and cannot use your TI tool.
Could you please…