Part Number: TAS5722L Other Parts Discussed in Thread: TAS2770 , TAS5805M , TAS2780 I am using TAS5722L which is an i2s-input amplifier. I can change the gain by register-setting over i2c. However a minimum gain ramp rate of 0.25dB per sample applies. I…
Part Number: TAS5722L We have on our board a TAS5722L. Unfortunately it doesn't work. Only a short crack noise comes from the speaker.
We suspect that the error is in the hardware, since we did the following test. We separated the I2C and only supplied…
Part Number: TAS5722L Hello,
We are using the TAS5722L and have the following questions:
- does this chipset have any power sequencing requirements?
- should SDZ be pulled-up or down? The EVM has it pulled up but we would like the amplifier to be disabled…
Part Number: TAS5722L Hello,
I was looking through the datasheet and Figure 5 caught my eye. For a supply voltage of 5V and a load of 4 Ohms, the maximum power is stated to be about 3W. How is this curve derived because assuming 100% efficiency, Power…
Part Number: TAS5722L Hello,
I am trying to find the dimensions for the component package of TAS5722LRSMR. It is TIs RSM 32 Package, but neither the datasheet nor the package drawing have an actual mechanical drawing. It just shows a 3d render of the component…
Part Number: TAS5722L Hi there, we had some questions regarding TAS5722L passive selection:
Input bulk capacitance:
Section 8.2 shows 2 x 100 uF electrolytic capacitors
Section 8.2.2.4 refers to them
The evaluation kit uses 2 x 47 uF electrolytic
Questions…