Part Number: TAS5733L Hi,
we are now quite some time failing to startup the TAS5733L Amplifier without having it set the error register bit for overcurrent/undercurrent or temperature fault, although everything we can measure seems within recommendations…
Part Number: TAS5733L
Is there any issue with PVDD dropping to 3.3V while shut down instead of 0v?
what sort of quiescent current could we expect in this configuration?
we are evaluating changes that would leave battery voltage on the PVDD rail to simplify…
Part Number: TAS5733L Other Parts Discussed in Thread: TAS5733 Hello,
Our customer also met the similar question as this, he used the internal oscillator to provide the MCLK, and SCLK is provided by blue tooth module, SCLK=48k*16*2=1.536Mhz, and MCLK is…
Part Number: TAS5733L I configure ADR/FAULT as output to see if the chip is overvoltage or undervoltage. When I input 3.3V AVDD to the chip, ADR/FAULT displays as 1, and the chip is working normally, but when I input PVDD After 12V, ADR/FAULT has been…
Part Number: TAS5733L Other Parts Discussed in Thread: TAS5805M Hi, Team
If i set the input signal to 0dBFS, and set all the others block function to 0dB, such as AGL, Volume, EQ.
what's the Maximum output voltage for TAS5733L(suppose PVDD is larger…
Part Number: PUREPATHCONSOLE
Tool/software:
A table with links to all the software needed for audio devices and their EVMs. Find the device(s) of interest in the table and use the links to request access to the software you need.
Product or Part …
Part Number: TAS5733L Tool/software: Linux Hi, I am using the TAS5733l Amp. But the channel 1 register gain (0x08) overwrite to 0x00 (from 0x00C0).
I am attaching the header file where i do the initialisation.
Anyone help why this value is overwrite…
Part Number: TAS5733L Other Parts Discussed in Thread: TAS5751M ,
During the test of TAS5733L/TAS5751M, we found that the high frequency signal part of TAS5733L/TAS5751M has a certain attenuation.
That is, after 10KHz, the output amplitude of the signal…
Part Number: TAS5733L Other Parts Discussed in Thread: TAS5733 Hi, Sir,
I will use 48KHz, 16Bit i2s, and no MCLK in,
How to config the Software code and Hardware?
1. MCLK and SCLK should be short??
2. Can support 32fs SLCK?
Part Number: TAS5733L Tool/software: Linux Hello,
We are using TI chip TAS5733L to design a soundbar. But we have some problems to solve.
1. We read the device ID register: it shows 0x41, not the default 0x40.
2. After init the control register like the…